How to use CodeWarrior TAP on LS1024ARDB

Document created by Bruce Tsai Employee on Jun 21, 2015Last modified by ebiz_ws_prod on Aug 6, 2018
Version 10Show Document
  • View in full screen mode

1. You should have CodeWarrior TAP(CWH-CTP-BASE-HE)and Probe Tips for LS1024A(CWH-CTP-VSPA-YE)

 

2. Install CodeWarrior for QorIQ LS Series ARMv7 ISA Windows v10.0.4

 

3. Install CodeWarrior patch (LS1024A-2MA_Windows_SP.zip)forLS1024/MA

1.png

4. Connect this tool to LS1024A RDB board and run CodeWarrior environment.

 

5.Start the bootloader and stop it at Barebox command line

 

6. In CodeWarrior environment File->New->Codewarrior Bareboard project wizard to add a LS1024A project.

    Run->Debug configuration->Debug

 

7. Window->Show View->Registers. Only ARM architecture registers you read here.

2.png

 

8. If you want to read peripheral device controller register, please use shell mode

   Window->Show->Debugger Shell

 

CodeWarrior Debugger
Shell v1.0

%> cmdwin::mem <device based address>+offset -s

3.png

(use command “help cmdwin::mem” to get the detail )

Attachments

Outcomes