Wire diagram for the TRK-MPC5604B

Document created by GUO XIAOLI Employee on Jul 12, 2012Last modified by johnmc on Jan 16, 2014
Version 4Show Document
  • View in full screen mode

Connection Diagram for TRK-MPC5604B to Rev. 1 Motor Control "Shield" Board


TRK_to_Shield_Connection.png


Connection Diagram for TRK-MPC5604B to Rev. 0 Motor Control Board TFC_ConnectorsAndCables.png

For the TRK-MPC5604, connect the flat ribbon cable to PortB as seen in the picture below.
Make the cable connections as shown below for dual motor with independent drive
connection

 

carkit5.jpg

Make the cable connections as shown below for dual motor with series drive connection

carkit6.jpg

Make the cable connections as shown below for Single motor connection

 

carkit7.jpg


Protect your electronics


1. Try not to stop the wheels while in motion.  This can cause current spikes.

2. Don’t disconnect or connect any cable when board is powered [ON].
3. Don’t discharge the battery below 5.5V
4. Don’t hit stationary objects

Attachments

    Outcomes