Connection Diagram for TRK-MPC5604B to Rev. 1 Motor Control "Shield" Board
Connection Diagram for TRK-MPC5604B to Rev. 0 Motor Control Board
For the TRK-MPC5604, connect the flat ribbon cable to PortB as seen in the picture below.
Make the cable connections as shown below for dual motor with independent drive
connection
Make the cable connections as shown below for dual motor with series drive connection
Make the cable connections as shown below for Single motor connection
Protect your electronics
1. Try not to stop the wheels while in motion. This can cause current spikes.
2. Don’t disconnect or connect any cable when board is powered [ON].
3. Don’t discharge the battery below 5.5V
4. Don’t hit stationary objects :smileyhappy:
The links to various images on this article is broken. Can we please have them fixed? Thanks.
What mean ENDL and ENDR???
Are the pins for activate the left dc motor( ENDL ) and activate the right dc motor (ENDR), if this is true, then the PWML and PWMR are the inputs pins for the input PWM signal for each dc motor respectively ????
greetings...