New P&E  ML  Universal  Adapter  not working with CW 7.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New P&E  ML  Universal  Adapter  not working with CW 7.2

1,894 Views
DK1BN
Contributor III

Hello ,

 

just got the new P&E ML Universal Adapter here and tried to use under CW 7.2 with MCF52259. Out of the box it was not working at all. After a firmware update it indicates correct erasing and programming but "verify" fails.

No chance for debugging. It seems to be that the programming was not correct. Anyone with similar experience?

With the P&E software package it seems to be working ....but not with CW 7.2.

Labels (1)
0 Kudos
Reply
2 Replies

1,677 Views
Britti1982
Contributor I

I had the same problem because I went from a P&E Debugger Rev C. to  REV D.

I addition to the request of the latest uint_cfz.dll version 3.59 made ​​to P&E saw that the problem can be resolved only by putting in series with the CLK line of the BDM a 22ohm smd from my hardware project and everything is working again properly.

This was also recommended by the MCF52259EVB.

I hope I was clear and help.

0 Kudos
Reply

1,677 Views
J2MEJediMaster
Specialist I

I suggest that you file a service request on that. Click here to file an on-line service request. When filing the request, select the category Software Product Support and the topic CodeWarrior.

 

---Tom

0 Kudos
Reply