native crash and low mem when take monkey test with LPDDR 4GB in imx8Mq evk
Hi,
our device use:
Android release is: p9.0.0_2.0.0-ga
Linux version 4.14.98
the uboot is 3GB in default, and we do changes to 4GB as blew:
1、use the MX8M_LPDDR4_RPA_v24.xlsx and datasheet to make .ds file;
2、use the mscale_ddr_tool_v3.10 to do stress test and generate the lpddr4_timing.c
3、copy the lpddr4_timing to uboot-imx\board\freescale\imx8mq_evk directory.
4、change the codes:
(1) add codes in imx8mq_evk.c
--- a/board/freescale/imx8mq_evk/imx8mq_evk.c
+++ b/board/freescale/imx8mq_evk/imx8mq_evk.c
@@ -97,6 +97,27 @@ int dram_init(void)
gd->ram_size = PHYS_SDRAM_SIZE - rom_pointer[1];
else
gd->ram_size = PHYS_SDRAM_SIZE;
+
+#if CONFIG_NR_DRAM_BANKS > 1
+ gd->ram_size += PHYS_SDRAM_2_SIZE;
+#endif
+
+
+ return 0;
+}
+
+int dram_init_banksize(void)
+{
+ gd->bd->bi_dram[0].start = PHYS_SDRAM;
+ if (rom_pointer[1])
+ gd->bd->bi_dram[0].size = PHYS_SDRAM_SIZE -rom_pointer[1];
+ else
+ gd->bd->bi_dram[0].size = PHYS_SDRAM_SIZE;
+
+#if CONFIG_NR_DRAM_BANKS > 1
+ gd->bd->bi_dram[1].start = PHYS_SDRAM_2;
+ gd->bd->bi_dram[1].size = PHYS_SDRAM_2_SIZE;
+#endif
return 0;
}
@@ -392,3 +413,11 @@ int get_imx8m_baseboard_id(void)
return IMX8M_REF_3G;
}
#endif
+
+phys_size_t get_effective_memsize(void)
+{
+ if (rom_pointer[1])
+ return (PHYS_SDRAM_SIZE - rom_pointer[1]);
+ else
+ return PHYS_SDRAM_SIZE;
+}
(2) add two banks in imx8mq_evk.h
--- a/include/configs/imx8mq_evk.h
+++ b/include/configs/imx8mq_evk.h
@@ -212,7 +212,9 @@
#define CONFIG_SYS_SDRAM_BASE 0x40000000
#define PHYS_SDRAM 0x40000000
#define PHYS_SDRAM_SIZE 0xC0000000 /* 3GB DDR */
-#define CONFIG_NR_DRAM_BANKS 1
+#define PHYS_SDRAM_2 0x100000000
+#define PHYS_SDRAM_2_SIZE 0x40000000 /* 1GB DDR */
+#define CONFIG_NR_DRAM_BANKS 2
and then build a firmware load into the device.
There is no error to use the mscale_ddr_tool_v3.10 do Calibration and stress test
*************************************************************************
ARM clock(CA53) rate: 800MHz
DDR Clock: 1600MHz
============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 4096MB
Total density detected on the board is: 4096MB
============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1600Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @200Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @50Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 2D-Training @1600Mhz...
[Process] End of initialization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Result] PASS
============ Step 2: DDR memory accessing... ============
Verifying DDR frequency [email protected]
Verifying DDR frequency [email protected]
Verifying DDR frequency [email protected]
[Result] OK
============ Step 3: DDR parameters processing... ============
[Result] Done
Success: DDR Calibration completed!!!
But when we use monkey test app to test, there is a native crash and low mem
Process: system_server
Subject: Low on memory -- 500MB total / 120MB system / 40MB systemui / 5MB WebViewLoader-arm64-v8a 5MB bluetooth / 40MB pinyin
Build: Android/kwe1901/kwe1901:9/2.0.0-ga-rc4/v0.0:userdebug/dev-keys
Low on memory:500MB.total$120MB.system$40MB.systemui$5MB.WebViewLoader-arm64-v8a$5MB.bluetooth:
at 40MB.pinyin(Foreground:0)
ntv ?? 51867: zygote (pid 9568) native
ntv ?? 46467: zygote64 (pid 9567) native
ntv ?? 28213: surfaceflinger (pid 3058) native
ntv ?? 11043: media.codec (pid 3079) native
ntv ?? 10443: audioserver (pid 9569) native
ntv ?? 7921: media.extractor (pid 3072) native
ntv ?? 6436: [email protected] (pid 9574) native
ntv ?? 5711: mediaserver (pid 9571) native
ntv ?? 5671: qca_wpa_supplicant (pid 3764) native
isPrevious: true
Build: Android/kwe1901/kwe1901:9/2.0.0-ga-rc4/v0.0:userdebug/dev-keys
Hardware: EVK
Revision: 0
Bootloader: unknown
Radio:
Kernel: Linux version 4.14.98-07251-g17818da-dirty (yangzhulin@ubuntu00) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #7 SMP PREEMPT Thu Apr 23 19:23:47 CST 2020
*** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
Build fingerprint: 'Android/kwe1901/kwe1901:9/2.0.0-ga-rc4/v0.0:userdebug/dev-keys'
Revision: '0'
ABI: 'arm64'
pid: 3190, tid: 3198, name: FinalizerDaemon >>> system_server <<<
signal 6 (SIGABRT), code -6 (SI_TKILL), fault addr --------
Abort message: 'decStrong() called on 0xf0563551f8e0 too many times'
x0 0000000000000000 x1 0000000000000c7e x2 0000000000000006 x3 0000000000000008
x4 feffef5550bb15b7 x5 feffef5550bb15b7 x6 feffef5550bb15b7 x7 7f7fff7f7fff7fff
x8 0000000000000083 x9 0000f05651bf9a68 x10 fffffff87ffffbdf x11 0000000000000001
x12 0000f056446439d0 x13 ffffffffffffffff x14 ffffffffff000000 x15 ffffffffffffffff
x16 0000f05651c322c8 x17 0000f05651b702d8 x18 0000f056446431ba x19 0000000000000c76
x20 0000000000000c7e x21 0000000000000083 x22 0000000012fc0788 x23 0000000012fc0788
x24 000000006fd9a680 x25 0000000012fcf8d8 x26 000000000000319b x27 0000f056503e0048
x28 0000f05644644588 x29 0000f056446438f0
sp 0000f056446438b0 lr 0000f05651b64a90 pc 0000f05651b64abc
backtrace:
#00 pc 0000000000021abc /system/lib64/libc.so (abort+124)
#01 pc 00000000000080f8 /system/lib64/liblog.so (__android_log_assert+296)
#02 pc 000000000000bdb8 /system/lib64/libutils.so (android::RefBase::decStrong(void const*) const+168)
#03 pc 000000000008ab04 /system/lib64/libgui.so (android::SurfaceControl::destroy()+132)
#04 pc 000000000008aa08 /system/lib64/libgui.so (android::SurfaceControl::~SurfaceControl()+32)
#05 pc 000000000008ab30 /system/lib64/libgui.so (android::SurfaceControl::~SurfaceControl()+16)
#06 pc 000000000000bd80 /system/lib64/libutils.so (android::RefBase::decStrong(void const*) const+112)
#07 pc 000000000010352c /system/lib64/libandroid_runtime.so (android::nativeRelease(_JNIEnv*, _jclass*, long)+76)
#08 pc 00000000003cd278 /system/framework/arm64/boot-framework.oat (offset 0x3cc000) (android.app.backup.BackupDataInput.dtor [DEDUPED]+152)
#09 pc 0000000000c5a3a8 /system/framework/arm64/boot-framework.oat (offset 0x3cc000) (android.view.SurfaceControl.finalize+104)
#10 pc 0000000000182664 /system/framework/arm64/boot-core-libart.oat (offset 0x78000) (java.lang.Daemons$FinalizerDaemon.doFinalize+100)
#11 pc 00000000001828ec /system/framework/arm64/boot-core-libart.oat (offset 0x78000) (java.lang.Daemons$FinalizerDaemon.runInternal+492)
#12 pc 000000000011085c /system/framework/arm64/boot-core-libart.oat (offset 0x78000) (java.lang.Daemons$Daemon.run+76)