Hello,
The on-chip 4MB memory is connected to the RT through the FlexSPI2 interface. So, accessing this memory it's the same as if you wanted to access an external flash memory. The memory that comes within the package is a Winbond W25Q32JV. For more details about the memory, please visit http://www.winbond.com. Additional to that, within the SDK you will find two examples named flexspi_nor_polling_transfer and flexspi_hyper_flash_polling_transfer. These two memories are also connected to the RT through the FlexSPI interface, so the procedure to follow is the same if you want to access the on-chip memory.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------