windows 10 iot boot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

windows 10 iot boot issue

3,944 Views
puneeth989
Contributor I

hi,

      I am trying to boot windows 10 iot on imx6q. But it is freezing in #KDTARGET: Refreshing KD connection. Please give any solution for this. I have attached the boot log.

Labels (1)
0 Kudos
Reply
2 Replies

3,776 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

May I ask, do you happen to get anything on your display?

You should see Windows logo after U-boot hands off to UEFI.

 

Message KDTARGET: Refreshing KD connection

This message is the Windows kernel debugger is attempting to connect over serial, which indicates you are making it into Windows. 

 

Thank you,

Best regards,

Aldo.

0 Kudos
Reply

3,776 Views
MengJu_Lin
NXP Employee
NXP Employee

nxf46838‌

I have a similar issue.

I use i.MX8M Mini EVK with W1860_1_0_1_NXPEVK_iMX8M_Mini_2GB_TestOEMInput-xml-Release.ffu flashed to SD card.

The attach files are screen shots of tera term and HDMI display.

It complains no IP address and stoppped. I don't have ethernet connection. How can I setup WIFI connection?tera term.PNGwindows.jpg

0 Kudos
Reply