My imx7d pico android things start kit died

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

My imx7d pico android things start kit died

9,197 Views
neuberfran
Contributor IV

Hi,

iI Connect a USB to serial adapter between the host PC and pico.

I Connect a USB cable between the OTG pico port and the host PC.

I can see my board with ls command or in COM port

But I can't do this iMX7D Pico won't boot  (steps 1 to 6 to restore original firmware and/or install android things

using setup normal jumpers  using android-things-setup-utility-windows soft

Pls, help me

Tags (1)
0 Kudos
Reply
7 Replies

8,472 Views
neuberfran
Contributor IV
0 Kudos
Reply

8,472 Views
neuberfran
Contributor IV
minicom -D /dev/ttyUSB0 not working
0 Kudos
Reply

8,472 Views
neuberfran
Contributor IV

How to I can know if my problem is in SOM or in board? Multimeter?

0 Kudos
Reply

8,472 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Neuber Sousa,

I’m not sure it if may be a driver problem. Have you checked if the Android Things Setup Utility works?

https://developer.android.com/things/hardware/imx7d

If this doesn’t help I would recommend reaching TechNexion as they manufactured the board and may be able to assist you better on how to determine if it’s a hardware problem or not.

Regards,

0 Kudos
Reply

8,472 Views
neuberfran
Contributor IV

I put multimeter in 5v and Gnd gpio and I get 5.01 to 5

04. I put multimeter in 3.3v and Gnd gpio and I get 3.37-3.38v.

I find this values too high in compare with Rpi

Em qua, 9 de out de 2019 19:19, gusarambula <[email protected]>

escreveu:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: My imx7d pico android things start kit died

reply from gusarambula

<https://community.nxp.com/people/gusarambula?et=watches.email.thread> in *i.MX

Processors* - View the full discussion

<https://community.nxp.com/message/1216798?commentID=1216798&et=watches.email.thread#comment-1216798>

0 Kudos
Reply

8,472 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Neuber Sousa,

The i.MX7D Pico board is manufactured and supported by TechNexion so I would recommend that you contact them especially in case you detect a hardware error.


That being said, I would recommend trying to restore an image by following the document below as it could be that the booting image is not correct, but it’s loaded and it’s not letting the board to enter serial downloader mode.
https://os.mbed.com/docs/mbed-linux-os/v0.7/first-image/pico-pi-baseboard-with-the-pico-imx7d-som.ht...

My apologies for the inconvenience.  I hope this helps,

Regards,

0 Kudos
Reply

8,472 Views
neuberfran
Contributor IV
sudo linux/imx_usb pico-imx7d_bootbomb_20170112.imx 

result: no matching usb device found
0 Kudos
Reply