i.MXRT1060 FlexIO3 access with DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1060 FlexIO3 access with DMA

Jump to solution
3,614 Views
antoinezen
Contributor III

On the iMXRT1060, the FlexIO periferal can normally be accessed using eDMA. But on the i.MX RT1060 user manual, in table "Table 3-3. DMA MUX Mapping" I can find no reference to FLEXIO3 but only FLEXIO1 and FLEXIO2.

Does that mean that the FLEXIO3 peripheral cannot be used with DMA?

or is something missing in the user manual ?

Thanks in advance!

/Antoine

0 Kudos
Reply
1 Solution
3,459 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Antoine Zen-Ruffinen

Does that mean that the FLEXIO3 peripheral cannot be used with DMA?

or is something missing in the user manual?

Yes, unfortunately, the FlexIO3 module is not accessible by the DMA peripheral, so you can only use the FlexIO1 and FlexIO2. Sorry for the inconvenience that this may cause you.

Best regards

Jorge Alcala

View solution in original post

0 Kudos
Reply
1 Reply
3,460 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Antoine Zen-Ruffinen

Does that mean that the FLEXIO3 peripheral cannot be used with DMA?

or is something missing in the user manual?

Yes, unfortunately, the FlexIO3 module is not accessible by the DMA peripheral, so you can only use the FlexIO1 and FlexIO2. Sorry for the inconvenience that this may cause you.

Best regards

Jorge Alcala

0 Kudos
Reply