Does MCUXpresso support NHS 3152?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MCUXpresso support NHS 3152?

Jump to solution
5,099 Views
kevin_fry
Contributor I

I tried installing MCUXpresso IDE 11.0.1_2563 and I installed the release_mra2_12_1_nhs3152 SDK

I installed the LPCxpresso plug in "com.nxp.nhs3xxx.update-7.9.2-SNAPSHOT-159" and tried to build the SDK projects but they fail and I don't see NHS3152 as an option in the processors section of the build config.

Tags (3)
0 Kudos
Reply
1 Solution
4,848 Views
lpcxpresso_supp
NXP Employee
NXP Employee

According to the NHS31xx documentation, "LPCXpresso IDE v8.2.2 is the supported IDE for developing with NHS31xx ICs".

Regards,

MCUXpresso IDE Support

View solution in original post

0 Kudos
Reply
3 Replies
4,848 Views
tillostermann
Contributor II

I'd love to see the NHS31xx MCUs supported in MCUXpresso as well. Need to run LPCXpresson on a virtual box guest machine having problems to connect after and virtual box upgrade. MCUXpresso native on Linux would solve that.

BR

0 Kudos
Reply
4,849 Views
lpcxpresso_supp
NXP Employee
NXP Employee

According to the NHS31xx documentation, "LPCXpresso IDE v8.2.2 is the supported IDE for developing with NHS31xx ICs".

Regards,

MCUXpresso IDE Support

0 Kudos
Reply
4,848 Views
lpcxpresso_supp
NXP Employee
NXP Employee

"Part support" patches of this nature produced for use with LPCXpresso IDE are not compatible with recent MCUXpresso IDE releases. You will need to use whatever IDE release is recommended by the NHS31xx documentation.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply