How To Use GPIO and CAN on i.MX8MM with Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Use GPIO and CAN on i.MX8MM with Yocto

Jump to solution
17,553 Views
dave_nugent
Contributor II

Hey,

I am having a bit of trouble trying to control GPIO pins and CAN on the i.MX8MM with Yocto. I can control pins using:

echo XX > /sys/class/gpio/export

echo "out" > /sys/class/gpio/gpioXX/direction
or
echo "in" > /sys/class/gpio/gpioXX/direction

echo 1 > /sys/class/gpio/gpioXX/value
or
echo 0 > /sys/class/gpio/gpioXX/value

echo XX > /sys/class/gpio/unexport

But I have not been able to find any information on how to actually set an exposed pin (like on the J1003 header). The only information I have seen is to make sure the DTS file is correct, but not how to actually set it, and to use i.MX Pins Tool v6. When I try to select my board in i.MX Pins Tool v6 I get the error

"Disk operation error. Check disk space and write permissions for data folder C:\ProgramData\NXP\mcu_data_v6"

Which does not make sense because I have over 200GB of free space in that disk and no weird write permissions. So I am really not sure where to go for the GPIO.

With the CAN I am able to get it all configured in the kernel, set up the CAN bitrate and start it, but I have no idea how to actually send a message. Any help or links to information would be greatly appreciated.

Thanks!

Dave

1 Solution
15,849 Views
jimmychan
NXP TechSupport
NXP TechSupport

For GPIO pins:

In the dts file, you can see there is the name of the pin and the iomux/pad setting of the pin.

fsl-imx8mm-evk.dts

For example:

MX8MM_IOMUXC_SAI2_RXC_GPIO4_IO22  0x19

"SAI2_RXC" is the real pin/pad of the i.MX8MM. The GPIO4_IO22 is one of the IOMUX functions of this pin. So, this setting means using the pin SAI2_RXC as a gpio pin gpio4_22.

The number 0x19 is the PAD CTL setting such as Pull enable/disable, Pull-up enable/disable, fast/slow slew rate and so on.

 

For details of MUX register, please read the i.MX8MM reference manual 8.2.5.105 Pad Mux Register (IOMUXC_SW_MUX_CTL_PAD_SAI2_RXC)

For details of PAD register, please read the i.MX8MM reference manual 8.2.5.259 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_SAI2_RXC)

 

Basically, all the pins are well defined in pins-imx8mm.h.So, you just pick up the correct pin name in the .h file. Then you can use the pin as gpio pin.

 

For the CAN, this may useful for you.

https://community.nxp.com/message/373598 

View solution in original post

5 Replies
15,849 Views
dave_nugent
Contributor II

Hey,

Jimmychan was very helpful, but I thought I would leave a comment with exactly how I got the gpio working as I wanted.

Some documentation on how to do this can be found in …/build-dir/tmp/work-shared/imx8mmevk/kernel-source/Documentation and in this document https://www.nxp.com/docs/en/user-guide/i.MX_BSP_Porting_Guide_Linux.pdf. Specifically to enable pin 37 on the expansion header we went to the dts file at .../build-dir/tmp/work-shared/imx8mmevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts and on line 322 changed:

MX8MM_IOMUXC_SAI5_RXD1_SAI5_RX_DATA1

to

MX8MM_IOMUXC_SAI5_RXD1_GPIO3_IO22

 

To set pad SAI5_RXD1 to be GPIO3_IO22 which we learned was a possibility from the IMXMM base board schematic page 16

 

We then went to line 884 and changed the status on the sai5 group from:

status = "disabled”;

to

status = "okay";

 

to enable the sai5 group

 

Then we ran BItbake –c menuconfig linux-imx to recompile the dts file and finally ran bitbake core-image-base to create a new image.

 

When that was all done we were able to set the GPIO over terminal with the commands:

 

echo 86 > /sys/class/gpio/export

echo "out" > /sys/class/gpio/gpio86/direction

echo 1 > /sys/class/gpio/gpio86/value

(86 because it is GPIO3_IO22, which in Linux means (3 - 1)*32 + 22 which is 86)

Hope that helps anyone else in a similar situation!

15,850 Views
jimmychan
NXP TechSupport
NXP TechSupport

For GPIO pins:

In the dts file, you can see there is the name of the pin and the iomux/pad setting of the pin.

fsl-imx8mm-evk.dts

For example:

MX8MM_IOMUXC_SAI2_RXC_GPIO4_IO22  0x19

"SAI2_RXC" is the real pin/pad of the i.MX8MM. The GPIO4_IO22 is one of the IOMUX functions of this pin. So, this setting means using the pin SAI2_RXC as a gpio pin gpio4_22.

The number 0x19 is the PAD CTL setting such as Pull enable/disable, Pull-up enable/disable, fast/slow slew rate and so on.

 

For details of MUX register, please read the i.MX8MM reference manual 8.2.5.105 Pad Mux Register (IOMUXC_SW_MUX_CTL_PAD_SAI2_RXC)

For details of PAD register, please read the i.MX8MM reference manual 8.2.5.259 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_SAI2_RXC)

 

Basically, all the pins are well defined in pins-imx8mm.h.So, you just pick up the correct pin name in the .h file. Then you can use the pin as gpio pin.

 

For the CAN, this may useful for you.

https://community.nxp.com/message/373598 

15,849 Views
dave_nugent
Contributor II

Thank you so much for the help!

I am still a little confused on a few things with the GPIO, firstly is there a document showing the connection between, for example, SAI2_RXC and an exposed pin on the board? I have found some information in the i.MX 8M Mini Hardware User's Guide 2.17, but it doesn't show alternate uses of each pin. Secondly, I am not sure where the .dts file I should edit is. I have found a .dts files that matches the one you linked  at: 

.../build-dir/tmp/work-shared/imx8mmevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts

on my host machine but when I edit it by changing line 142  from

MX8MM_IOMUXC_GPIO1_IO14_CCMSRCGPCMIX_CLKO1 0x59

to

MX8MM_IOMUXC_GPIO1_IO14_CCMSRCGPCMIX_CLKO1 0x58

to try and select 000 ALT0 — Select signal GPIO1_IO14 as described in i.MX 8M Mini Reference Manual 8.2.5.20

then I run bitbake core-image-base, and flash the SD card

from there I try to set the GPIO as described above (with the XX replaced with 14) and check on pin  31 on J1003 but it did not work.

Do you have any ideas of what I am doing wrong? I have seen some references to rebuilding the .dts file, how would I do that?

Thanks again!

Dave

0 Kudos
Reply
15,849 Views
jimmychan
NXP TechSupport
NXP TechSupport

You can check the schematic of the i.MX8MM-EVK board. You can download it from here:

i.MX 8M Mini Evaluation Kit | NXP 

For the IOMUX setting (alternate uses) of each pin, please read the i.MX8MM Reference Manual. You can download it from here:

i.MX 8M Mini Applications Processor | Arm Cortex A53/M4 | 1080P display | NXP 

If you want to use the GPIO1_IO14 pin as gpio pin, please change it to GPIO1_IO14 in dts file.

MX8MM_IOMUXC_GPIO1_IO14_GPIO1_IO14   
15,850 Views
Chayma
Contributor III

hello,

I am using imx8mm and i want to activate and configure ecspi1 pinout on the expansion connector. Could someone help me please.

Best regards,

0 Kudos
Reply