Difference between "vpudec" and "imxvpudec"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between "vpudec" and "imxvpudec"?

7,727 Views
shiva_mudugal
Contributor I

Hi All,

 

What is the difference between "vpudec" and "imxvudec". I also observer that some avi files doesn't work with "imvpudec" when we play using "playbin", we get below error.

But the same file works with "vpudec". Any help would be much appreciated. Am using below version of gstreamer-imx

 

Name imxvpu
Description video en- and decoder elements using the Freescale i.MX VPU
Filename /usr/lib/gstreamer-1.0/libgstimxvpu.so
Version 0.12.2
License LGPL
Source module gstreamer-imx
Binary package Unknown package release
Origin URL Unknown package origin

 

 

 

root@imx6dlsabrebavn:~# gst-launch-1.0 playbin uri=file:///media/usb/F2F4-0D11/test/videoUSB/MusicVideo/BLACKPINK\ -\ \'FOREVER\ YOUNG\'\ FMV.avi video-sink="imxipuvideosink alpha=0"
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...

====== AIUR: 4.1.4 build on Sep 10 2018 09:55:25. ======
Core: AVI_PARSER_03.05.26 build on Aug 12 2016 06:15:51
file: /usr/lib/imx-mm/parser/lib_avi_parser_arm11_elinux.so.3.1
------------------------
Track 00 [video_0] Enabled
Duration: 0:04:04.827916000
Language: und
Mime:
video/mpeg, systemstream=(boolean)false, parsed=(boolean)true, mpegversion=(int)2, width=(int)800, height=(int)480, framerate=(fraction)24000/1001
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:04:04.897959000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, channels=(int)2, rate=(int)44100, bitrate=(int)0
------------------------
ERROR: from element /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstAiurDemux:aiurdemux0: GStreamer encountered a general stream error.
Additional debug info:
../../../imx-gst1.0-plugin-4.1.4/plugins/aiurdemux/aiurdemux.c(1015): aiurdemux_pull_task (): /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstAiurDemux:aiurdemux0:
streaming stopped, reason not-negotiated, state 3
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...

 

 

 

-Regards

Shiva Kumar M S##@

Labels (2)
0 Kudos
Reply
4 Replies

6,255 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shiva

difference between "vpudec" and "imxvudec" is that first is part nxp imx-gst1.0-plugins,

its usage can be found in linux official documentation (Linux Guide) on

i.MX Software|NXP 

imxvpudec is part of gstreamer-imx plugins developed and supported by community:

GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,255 Views
shiva_mudugal
Contributor I

Hi igorpadykov‌,

Thanks for the response. Do you mean to say that "imxvpudec" is not part of the official NXP supported plugins?. "gstreamer-imx" is not maintained by nxp?

-Regards,

Shiva Kumar M S

0 Kudos
Reply

6,255 Views
igorpadykov
NXP Employee
NXP Employee

right

Best regards
igor

0 Kudos
Reply

6,254 Views
igorpadykov
NXP Employee
NXP Employee

right, "imxvpudec" is not part of the official NXP supported plugins.

NXP offical (supported ) plugins are listed in oficial NXP documentation, please refer to

attached Release Notes Table 24. Freescale GStreamer 1.0 plugins.

imxvpudec is part of gstreamer-imx plugins developed and supported by community:

GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms

Best regards
igor

0 Kudos
Reply