Installing GStreamer on I.MX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing GStreamer on I.MX8QM

8,965 Views
mustafa_ozcelik
Contributor I

Hi all,

I am trying to figure out how to properly install gstreamer on imx8qm-mek (for a qt app to use).
I am using the morty branch (beta2 release) for imx8qm.
More precisely Linux L4.9.51 for i.MX 8QuadMax Beta2 and i.MX 8QXPlus Beta  from Alpha / Beta BSPs for Microprocessors|NXP . And I am building an image with weston/wayland.
I have the following in my image recipe:

IMAGE_INSTALL_append = " qtmultimedia \

gstreamer1.0 \

gstreamer1.0-plugins-base \

gstreamer1.0-plugins-bad \

packagegroup-gsl-gstreamer1.0 \

gstreamer1.0-plugins-base-meta \

gstreamer1.0-plugins-bad-meta \
gstreamer1.0-plugins-good-meta \
libnl \

libnl-genl \

qtbase-plugins \

qtmultimedia-plugins \

qtimageformats-plugins \

"


When I create the image, qt media player app (which works in Raspberry Pi) complains:

====== BEEP: 4.3.3 build on Aug 13 2018 18:58:20. ======
Core: AAC decoder Wrapper build on Dec 7 2017 18:13:51
file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm_elinux.so.3
Warning: "No decoder available for type 'video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1280, height=(int)720, framerate=(fraction)25/1, codec_data=(buffer)014d401fffe1001c674d401fe8802802dd80b501010140000003004000000c83c60c448001000468ebef20, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, profile=(string)main, level=(string)3.1'."
CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.09.00_ARMV8 build on Sep 20 2017 15:02:50.
====== BEEP: 4.3.3 build on Aug 13 2018 18:58:20. ======
Core: MP3 decoder Wrapper build on Dec 7 2017 18:14:28
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm_elinux.so.3
CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_ARMV8 build on Feb 13 2017 19:47:36.
====== AIUR: 4.3.3 build on Aug 13 2018 18:58:16. ======
Core: MPEG4PARSER_06.12.12 build on Oct 27 2017 02:58:02
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2
------------------------
Track 00 [video_0] Enabled
Duration: 0:03:58.600000000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1280, height=(int)720, framerate=(fraction)25/1, codec_data=(buffer)014d401fffe1001c674d401fe8802802dd80b501010140000003004000000c83c60c448001000468ebef20
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:03:58.608244000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)0, stream-format=(string)raw, codec_data=(buffer)1210
------------------------

Furthermore, I get the following (which I was able to get rid off by removing gst- plugins (not the gstreamer1.0 ones)

(gst-plugin-scanner:9753): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-1.0/libgstqt5videosink.so': libXdamage.so.1: cannot open shared object file: No such file or directory

Now, I noticed that in the master branch of meta-freescale, there are some new recipes under gstreamer folder, namely: gstreamer1.0-plugins-imx gstreamer1.0_1.12.imx. I am unable to integrate these because of the syntax changes in Yocto from morty to rocko. Are these packages important. Is it sufficient to have morty release for a complete gstreamer install?

Any suggestions are highly appreciated.

0 Kudos
Reply
7 Replies

6,584 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems you haven't add vpu decoder in the bsp, one can try to install libav (software decoder).


The following steps show how to install gstreamer1.0-libav into a rootfs image.
1. Add the following lines into the configuration file conf/local.conf.
IMAGE_INSTALL_append = " gstreamer1.0-libav"
LICENSE_FLAGS_WHITELIST = "commercial"
2. Build gstreamer1.0-libav.
$ bitbake gstreamer1.0-libav
3. Build the rootfs image.
$ bitbake
$ <image_name>

0 Kudos
Reply

6,584 Views
mustafa_ozcelik
Contributor I

Hi,
I tried this today without nowing it is the software decoder.
There is some improvement, yes. Now I can at least see the player work, however there is 80% of the time black screen. 20% of the time I see the flickering images of the movie.

Can I assume that is it because the software decoder isn't fully supported efficiently?
Is it maybe because I have to include other decoders such as AAC+ etc from external repositories?

I think i.MX8QM does not fully support multimedia related things just yet.

The following is from release notes:

6.4 Known issues and limitations for multimedia
Issues seen on GStreamer 1.x:
• As the maximum buffer size of the playbin multiqueue is 2 MB, problems may be seen with some long audio or video
interleaved streams. You can enlarge this buffer size to support these special use cases.
• AAC decoder: The ADIF format does not support seek mode nor FF/FB.
• The accurate seek mode may have a longer time delay.
• Because the stream container does not have an index table, seeking is not supported.
• Fast rewind of audio does not support audio-only streams.
• Pulseaudio is only available for the X11 backend.
• Rewind may report an EOS when using libav for video decoding.






For the clips with long audio/video interleaved streams, it requires to enlarge the multiqueue maximum buffer size.
AAC clips with ADIF format do not support seek/trick (FB/FF) mode.
Accurate seek mode may take a longer time delay.
For clips with no index table in containers (or video with only very few key frames), seeking is not supported.
Audio-only clips do not support FB.
For pulseaudio, it automatically starts with X11 backend. For others, users need to manually start the daemon.

What else could I try?
Thank you very much for the information

0 Kudos
Reply

6,584 Views
mustafa_ozcelik
Contributor I

Okay, now I tried using gst-play-1.0, it works.
My Qt app has something to do with the current issue. Do you know any methods I could try to make QtMultimedia use this correctly?

Full image recipe is below:

#Sound related
DISTRO_FEATURES_append = " pulseaudio "

IMAGE_INSTALL_append = "  alsa-lib \
                          alsa-tools \
                          alsa-state \
                          pulseaudio \
                          imx-alsa-plugins \
"

# Qt dependencies for infotainment application
IMAGE_INSTALL_append = " qtconnectivity qtquickcontrols2 \
                         qtvirtualkeyboard qtwebsockets \
                         qtmultimedia     qtbase-tools \
                         qtbase-plugins \
                         qtdeclarative \
                         qtdeclarative-tools \
                         qtdeclarative-qmlplugins \
                         qtmultimedia \
                         qtmultimedia-plugins \
                         qtmultimedia-qmlplugins \
                         qtsvg \
                         qtsvg-plugins \
"

# Gstreamer and its plugins
# gstreamer1.0-plugins-imx is not compatible with imx8 at the moment! Add it also..
#IMAGE_INSTALL_append = " imx-vpu imx-vpuwrap   "
IMAGE_INSTALL_append = " imx-codec imx-parser v4l-utils imx-gst1.0-plugin imx-alsa-plugins"
#IMAGE_INSTALL_append = " imx-aacpcodec imx-mscodec imx-msparser imx-ac3codec imx-ddpcodec imx-real imx-hifi4 imx-hifi4-aacp "

IMAGE_INSTALL_append = " gstreamer1.0 \
                         gstreamer1.0-plugins-base \
                         gstreamer1.0-plugins-good \
                         gstreamer1.0-plugins-bad \
"

IMAGE_INSTALL_append = " packagegroup-fsl-gstreamer1.0 gstreamer1.0-plugins-base-meta  gstreamer1.0-plugins-good-meta gstreamer1.0-plugins-bad-meta "

IMAGE_INSTALL_append = " gstreamer1.0-libav ffmpeg"

#IMAGE_INSTALL_append = " gstreamer1.0-omx "

IMAGE_INSTALL_append = " libnl libnl-genl \
                         qtbase-plugins \
                         qtmultimedia-plugins \
                         qtimageformats-plugins  \
                         qtmultimedia-qmlplugins \
"

IMAGE_INSTALL_append = " packagegroup-fsl-tools-testapps "

# Geoclue
IMAGE_INSTALL_append = " geoclue "

Thank you very much again.

0 Kudos
Reply

6,585 Views
dan_searles
Contributor I

Hello,

Could you give name, location and any needed references for the above mentioned "Full image recipe"?

Thanks

0 Kudos
Reply

6,585 Views
joanxie
NXP TechSupport
NXP TechSupport

what is qt app issue? if you play the AAC+ file, you need the special codec package which is under NDA.

0 Kudos
Reply

6,585 Views
mustafa_ozcelik
Contributor I

Sorry for confusing question. I have a problem using GStreamer + QtMultimedia on iMX8. This might be out of scope for this forum, but here is the question if anybody would like to help.

qt - Asking QtMultimedia to use different video sink using QML - Stack Overflow 

Thanks

0 Kudos
Reply

6,585 Views
joanxie
NXP TechSupport
NXP TechSupport

one can use qtmultimdia(qlmvideo) to playback video by VPU, try to add gstreamer into qtmultimeda like this:

PACKAGECONFIG_append_pn-qtmultimedia = "gstreamer" in the lcoal.conf

0 Kudos
Reply