Hello I am devolping a Qt app for a imx6 freescale microprocessor. I am using qtcreator 4.2.1.
I need to use the SPI module of imx6. At firs I build a 3.14 kernel version and I made a program bassed of spidev_test example. My program is:
First SPI configuration:
int ret = 0;
device = "/dev/spidev0.0";
bits = 8;
speed = 4500000;
mode = 0;
delay = 0;
fd = open(device, O_RDWR);
if (fd < 0){
pabort("can't open device");
}
else{
qDebug("Open device");
}
/*
* spi mode
*/
ret = ioctl(fd, SPI_IOC_WR_MODE, &mode);
if (ret == -1){
pabort("can't set spi mode");
}
ret = ioctl(fd, SPI_IOC_RD_MODE, &mode);
if (ret == -1){
pabort("can't get spi mode");
}
/*
* bits per word
*/
ret = ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits);
if (ret == -1){
pabort("can't set bits per word");
}
ret = ioctl(fd, SPI_IOC_RD_BITS_PER_WORD, &bits);
if (ret == -1){
pabort("can't get bits per word");
}
/*
* max speed hz
*/
ret = ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed);
if (ret == -1){
pabort("can't set max speed hz");
}
ret = ioctl(fd, SPI_IOC_RD_MAX_SPEED_HZ, &speed);
if (ret == -1){
pabort("can't get max speed hz");
}
qDebug("spi mode: %d\n", mode);
qDebug("bits per word: %d\n", bits);
qDebug("max speed: %d Hz (%d KHz)\n", speed, speed/1000);
Then the transfer function:
void SpiCom::transfer(int fd, unsigned char word){
int ret;
uint8_t rx[] = {0, };
spi_ioc_transfer tr;
unsigned char data[] = {word};
tr.tx_buf = (unsigned long)data;
tr.rx_buf = (unsigned long)rx;
tr.len = 1;
tr.delay_usecs = delay;
tr.speed_hz = speed;
tr.bits_per_word = bits;
ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr);
if (ret < 1)
pabort("can't send spi message");
dataReaded = (unsigned char)rx[0];
}
With 3.14 version kernel my program works well but I had to update to a 4.9 kernel version and then my program doesn't work. When I want to transfer data always show "can't send spi message" message error.
If I compile this part of program with gcc compiler works but when I use qt compiler and execute the app It shows message error.
I am searching for everywhere but I couldn't find nothing.
If someone can help me.