MCUXpresso v10.1.1.606 - hangs at 2% when debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso v10.1.1.606 - hangs at 2% when debugging

Jump to solution
1,899 Views
mathieu_bordere
Contributor I

Setup is an i.MX RT1050 board connected with a j-link Segger interface.

When opening MCUXpresso and launching a Debug session, the debug session starts within an acceptable timeframe, however, if I stop the debug session and restart it, launching of the debug session will hang at 2% completion and can stay there for a 60+ sec before continuing.

My current solution is exiting and restarting MCUXpresso because that is actually faster than trying to launch a debug session for a second time.

Any help is appreciated.

Kind regards,
Mathieu

0 Kudos
Reply
1 Solution
1,793 Views
BlackNight
NXP Employee
NXP Employee

Hi Mathieu,

I don't remember that I saw someting like this. Have you tried the MCUXpresso 10.2 already?

The 10.2 includes updated debugger and update J-Link files, so your problem might be solved with this?

Erich

View solution in original post

0 Kudos
Reply
2 Replies
1,794 Views
BlackNight
NXP Employee
NXP Employee

Hi Mathieu,

I don't remember that I saw someting like this. Have you tried the MCUXpresso 10.2 already?

The 10.2 includes updated debugger and update J-Link files, so your problem might be solved with this?

Erich

0 Kudos
Reply
1,793 Views
mathieu_bordere
Contributor I

Indeed, upgrading solves the issue!

0 Kudos
Reply