Hello Gary,
You are right. My mistake. The information that the gc7000lite gpu core has 800MHz max clock came from our experts. Let me double check with them to see what information is correct. The i.MX8M Datasheet (Rev. 0.1, 05/2018) does specify a nominal and an overdrive mode:
Nominal mode—the maximum GPU frequency supported in this mode is 800 MHz.
Overdrive mode—the maximum GPU frequency supported in this mode is 1 GHz.
So perhaps the BSP uses the nominal mode while the overdrive is also valid. Let me also check why would only 800Mhz be implemented.
I'll keep you informed.
Regards,
Gustavo