RT1050 Crystal Spec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 Crystal Spec

2,558件の閲覧回数
martinsmith
Contributor III

Hi, I'm looking for an exact spec for the xtal on the RT1050. The datasheet gives a bit of a incomplete spec. Would the crystals mentioned in this thread do the job? https://community.nxp.com/thread/308944  

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,328件の閲覧回数
martinsmith
Contributor III

Thanks Igor, I have selected the FA-20H 24.0000MF20X-K3 from Epson which I think meets all the requirements.

0 件の賞賛
返信

2,328件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

since i.MX and Vybrid parts use many same IP modules and particular XTALOSC,

crystals mentioned on that thread also can be used with RT1050. Seems most full

characteristics are given in Table 9. Recommended External Crystal Specifications

i.MX25 Datasheet

https://www.nxp.com/docs/en/data-sheet/IMX25CEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信