i.MX8M EVK MIPI CSI Camera Frame Rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M EVK MIPI CSI Camera Frame Rate

29,344 Views
felixradensky
Contributor IV

Hello,

We have purchased NXP MIPI-CSI camera MINISASTOCSI kit and followed the instructions in this application note https://www.nxp.com/docs/en/application-note/AN12187.pdf  to test the camera on NXP i.MX8M EVK rev B3 running L4.9.51-ga Linux BSP release. Both camera connectors were tested. The camera output was sent to HDMI display. The frame rate we've received is around 7fps, even in lowest resolution. What should be done to get the maximum frame rates advertised by the application note above (e.g. 30fps at 1080p).

Thanks.

Felix.

Labels (2)
26 Replies

22,459 Views
chunfengren
Contributor I

HI, Tom zheng

thanks for your patch you provide,  it work very well now.

if use 640*480 resolution to take video of moving object, recorded video is very clear and the video quality is good.

if use 1280*720(or 1920*1024) to take video of moving object, video is very  blur and the video quality isn't good.

is it be affected by no vpu in i.MX8M EVK?

How do I solve it?

thanks a lot

0 Kudos
Reply

22,459 Views
haidong_zheng
NXP Employee
NXP Employee

Yes, i.MX8M does not have HW video encode. so, video encode is done by SW. If high FPS is needed in high resolution. Some encode simply and optimize are needed done by customer. 

0 Kudos
Reply

22,458 Views
chunfengren
Contributor I

HI,Tom zheng

Thanks for your reply.

Do you have similar image encode code patch to support high resolution recording?

0 Kudos
Reply

22,458 Views
haidong_zheng
NXP Employee
NXP Employee

no ,thanks! 

0 Kudos
Reply

22,567 Views
chunfengren
Contributor I

I meet a similiar problem:

We have purchased NXP MIPI-CSI Ov5640 camera,
and we do camera test on NXP i.MX8M EVK, The camera output was sent to HDMI display.
when we preview and take video on ov5640, and  take video of  moving objects, video is very  blur.

from kernel logs to see , there is many RX fifo overflow, it make some  captured Frames by camera lost.

[  867.956960] mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Rx fifo overf
low
[  870.956451] mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Rx fifo overf
low
[  874.273032] mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Rx fifo overf
low 

0 Kudos
Reply

22,564 Views
haidong_zheng
NXP Employee
NXP Employee

"rx fifo over flow" is another topic.

If you can, please carefully apply another two packages patches. 

One package(tuning.7z) include ATF, u-Boot, Kernel patches for DDR.

Another package(Camera.tar.bz2) include CSI driver patches. 

Two packages must be applied on GA release for this problem. 

If you still meet the "rx fifo over flow" after those packages merged, please tell us how to repeat it and show us the log info. 

Thanks! 

22,515 Views
vsuneja63
Contributor III

Hi Tom,

I am facing same "rx fifo overflow" error with MINISASTOCSI camera. I am trying to apply attached patches but its failing. I am using

kernel 4.19.35

u-boot-imx-2019.04

Does these patches will work with these system configuration on imx8mq-evk target?

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply

22,453 Views
haidong_zheng
NXP Employee
NXP Employee

Hi Suneja:

The SDK is & after 4.14.78 already inlcuded theose patches.

0 Kudos
Reply

22,563 Views
jobusch
Contributor I

Hello Tom,

thank you for providing these patches. We have a similar problem. We get FIFO_RX_overflow error too. But only when we have high cpu usage at the same time. So thats why your "tuning" patches seem perfect. But they do not fit my version. I am running 4.14.78. On which GA version are the patches made for?

0 Kudos
Reply

22,561 Views
haidong_zheng
NXP Employee
NXP Employee

Busch:

4.14.78 should already include those patches.

0 Kudos
Reply

22,556 Views
jobusch
Contributor I

Do you have any other idea, how to fix RX FIFO Overflow errors then?

0 Kudos
Reply

22,556 Views
haidong_zheng
NXP Employee
NXP Employee

Johannes:

@Liu Liu<mailto:[email protected]> could you share your idea about this ?

0 Kudos
Reply

22,556 Views
weiping_liu
NXP Employee
NXP Employee

Hi Tom,

The recommended workaround for this erratum is to avoid MIPI CSI overflow happen. Two undocumented debug registers can be used to monitor CSI FIFO levels in real time. When FIFO reaches one threshold, disable CSI and restart CSI.

For example, create one program on M4 core to monitor CSI FIFO level and do as follows:

  1. Read the CSI FIFO debug registers: Register CSI1_CSICR19 (0x30A9_004C) for MIPI CS1 or register CSI2_CSICR19 ( 0x30B8_004C) for MIPI CSI2
  2. If  the value of register CSIx_CSICR19 is larger than 192, Set register CSI_PHY_CTL_REG (0x30A7_0104 for MIPI CS1 or 0x30B6_0104 for MIPI CSI2) as 0xff to restart CSI.
  3. Wait for 3us. Jump to step 1).
0 Kudos
Reply

17,163 Views
martintso
Contributor I

Hi, Weiping

  We use I.MX8MQ and have two CSI input to capture video in (use LT6911C , two HDMI in to two LT6911C CSI output to I.MX8MQ). input video format is 1080P, 30FPS. Android 11 OS. Then display from I.MX8MQ DSI port into LCM panel.

  And by current test result.

1.MIPI-CSI#1 seems ok, can display over two hours.

2.MIPI-CSI#2 is NG, around several minutes happens RX FIFO overflow.

 Would like to know is there any difference in HW path/architecture, or SW (resource allocation) between  MIPI-CSI#1 and MIPI-CSI#2.

  Many thanks. 

  Martin 

 

0 Kudos
Reply

22,558 Views
james_kim
Contributor II

Thanks Tom,

It really helped me. 

James

0 Kudos
Reply

22,559 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Felix,

Did it work for you as well?

0 Kudos
Reply

22,559 Views
felixradensky
Contributor IV

Hi,

Yes it works for me. It was me posting as Ofer Austerlitz.

Thanks.

Felix.

22,559 Views
felixradensky
Contributor IV

Hello Lily,

With eMMC patches applied and number of buffers increased we get 18fps at 1080p

Felix

0 Kudos
Reply

22,559 Views
haidong_zheng
NXP Employee
NXP Employee

hi Felix:

Please check FPS by below command:

gst-launch-1.0 v4l2src ! video/x-raw,width=1920,height=1080 ! fpsdisplaysink

And please enable dma-coherent in fsl-imx8mq.dtsi for csix_bridge:

csi1_bridge: csi1_bridge@30a90000 {
compatible = "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x0 0x30a90000 0x0 0x10000>;
interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_CSI1_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
dma-coherent;
status = "disabled";
};

csi2_bridge: csi2_bridge@30b80000 {
compatible = "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x0 0x30b80000 0x0 0x10000>;
interrupts = <GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_CSI2_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
dma-coherent;
status = "disabled";
};

22,559 Views
oferausterlitz
Senior Contributor II

Hi Tom,

After adding dma-coherent property we get about 30fps at 1080p, which is great. We've also tested maximum resolution, 2592x1944 and received the following error:

0:00:00.643195654   510      0xff16ca0 ERROR         v4l2bufferpool gstv4l2bufferpool.c:854:gst_v4l2_buffer_pool_start:<v4l2src0:pool:src> we received 6 buffer from device '/dev/video0', we want at least 7

With DMA coherency enabled, is it necessary to increase GST_V4L2_MIN_BUFFERS to 7 ? Can this parameter be modified at run-time instead of compile-time ?

Thanks a lot.

Felix.

0 Kudos
Reply