PN7462 FW and SW examples full (NDA) version incomplete?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 FW and SW examples full (NDA) version incomplete?

ソリューションへジャンプ
3,126件の閲覧回数
jarojuda
Contributor II

I downloaded Sw368319 - PN7462AU FW And SW Examples Full Version - V05_12_00 (1.9) from docstore.

The package PN7462AU-FW_v05.12.00_Extended.zip seems corrupted.

 No example involving MIFARE DESFIRE compiles. The other examples compile well. 

There are unresolved dependencies from phalMfdf.h (the log attached).

I noticed that files from the phalMfdf component differs from that I have downloaded in Sw375617 - NFC Reader Library V05.12.00 Including MIFARE DESFire, MIFARE Plus And ICODE DNA Modules (1.7).

I replaced the MIFARE DESFIRE component in the PN7462 Extended by that from  Sw375617 and now all examples compiles.

Did any of you have a similar problem?

ラベル(2)
タグ(1)
1 解決策
2,633件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Jaroslaw,

There is a updated version available on docstore, would you please try it?

pastedImage_2.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,506件の閲覧回数
thiago_machado
Contributor III

Hi. I just downloaded the PDF file containing all the files, but it's for a passwork in order to open the PDF file. How can I get this password?

0 件の賞賛
返信
2,634件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Jaroslaw,

There is a updated version available on docstore, would you please try it?

pastedImage_2.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------