NFC USB Dongle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC USB Dongle

3,546 Views
nicoladegani
Contributor I

Hello,

I bought the "NFC USB Dongle" MIKROE-2540. I would like to know if someone has already start to use this device, and how it works. 

It is possible to send commands by "command prompt" to this device?

Do you have some examples software?

Thank you in advance

Best regards

Nicola

0 Kudos
Reply
1 Reply

2,832 Views
rainersabelka
Contributor I

On Linux you can use GitHub - NXPNFCLinux/linux_libnfc-nci: Linux NFC stack for NCI based NXP NFC Controllers 

There is a demo application included.

Just make sure you configure the library with --enable-pn7150 and --enable-lpcusbsio

Regards,

-Rainer

0 Kudos
Reply