Implementation of "Wi-Fi Access Point" on IMX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementation of "Wi-Fi Access Point" on IMX7

2,920 Views
vikram_bidkar
Contributor I

Dear All,

I am trying to implement "Wi-Fi Access Point" on the IMX7 evaluation board having Murata Wi-Fi chip(LBEH5HMZPC).

Below are my changes in .config file.

CONFIG_BCMDHD_FW_PATH="/lib/firmware/bcm/ZP_BCM4339/fw_bcmdhd_apsta.bin"
CONFIG_BCMDHD_NVRAM_PATH="/lib/firmware/bcm/ZP_BCM4339/bcmdhd.ZP.SDIO.cal"

CONFIG_HOSTAP=y
CONFIG_HOSTAP_FIRMWARE=y

but when I do "ifconfig wlan0 up" I am getting following error

root@imx7dsabresd:~# ifconfig wlan0 up

Dongle Host Driver, version 1.141.92 (r)
Compiled in drivers/net/wireless/bcmdhd
wl_android_wifi_on in
mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
mmc1: queuing unknown CIS tuple 0x80 (6 bytes)
F1 signature OK, socitype:0x1 chip:0x4339 rev:0x1 pkg:0x0
DHD: dongle ram size is set to 786432(orig 786432) at 0x180000
dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
dhd_bus_rxctl: resumed on timeout, INT status=0x208000C0
dhd_bus_rxctl: rxcnt_timeout=1, rxlen=0
dhd_check_hang: Event HANG send up due to re=1 te=0 e=-110 s=2
dhd_open : wl_android_wifi_on failed (-14)

What could be the issue?

Note: Wi-Fi is working fine in client mode. It can able to scan and all.

0 Kudos
Reply
3 Replies

2,287 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vikram

please refer to additional documentation (probably you will have to ask access to it

using murata support portal : wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html)

Murata Wi-Fi & BT Solution for i.MX Quick Start Guide (Linux) 4.0.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,287 Views
vikram_bidkar
Contributor I

Thank you very much igor.

Sorry for the late response.

"Murata i.MX Linux 4.1.15_2.0.0" Quick Start Binary Patch Release does not contain bcm firmware file. It has only NVRAM file(bcmdhd.1CK.OOB.cal and bcmdhd.1CK.SDIO.cal ). Please let me know where can I get the proper bcm firmware file for Wi-Fi chip LBEH5HMZPC ( Access Point mode).

Thanks and regards,

Vikram

0 Kudos
Reply

2,287 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vikram

for additional bcm files one can apply to Murata support, link
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor

0 Kudos
Reply