Pokitto LPC11U68 Game Gadget on Kickstarter - EB sold out soon!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pokitto LPC11U68 Game Gadget on Kickstarter - EB sold out soon!

2,860 Views
pokitto
Contributor I

Hello all LPC fanboys.

Fancy debugging something fun for a change? Pokitto, a DIY opensource game console is hitting 80% in less than 2 days on Kickstarter.

Pokitto is an amazing little device: a single ARM Cortex-M0+ driving a color 2.0" TFT at speeds like there is no tomorrow. 2x audio outputs, massive 18 GPIO extension header, 600 mAh li-po with built in charger... its a beauty!

If you want an earlybird kit @ 39 USD you better go check it out now, 69 units only left.

Kickstarter

http://kck.st/2oIzIYm

Webpage

http://bit.ly/2pg2BK9

Youtube video

http://bit.ly/2qpHti5

Thank you!

Jonne

0 Kudos
Reply
1 Reply

1,333 Views
bevisandrew
Contributor I

The Pokitto sounds like an exciting project, and I can’t wait to see how it evolves. I’ve been working on some fun projects myself, including a game called block breaker, which has really pushed my creativity. Best of luck with the Kickstarter campaign—it's great to see such innovative devices coming to life!

0 Kudos
Reply