Flash protection S32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash protection S32k144

Jump to solution
5,828 Views
lohrsistemas
Contributor IV

Hi,

How do I program the options bytes to protect the flash reading?

Thanks.

1 Solution
5,046 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

In this case, change the FSEC byte. Default value is 0xFE which means the device is not secured (you can access everything via JTAG). Last two bits say if the device is secured or not:

pastedImage_1.png

Change the value from 0xFFFF7FFE to 0xFFFF7FFC or 0xFFFF7FFD or 0xFFFF7FFF and the device will be secured. You can enable backdoor key access if needed.

Regards,

Lukas

View solution in original post

4 Replies
5,046 Views
lohrsistemas
Contributor IV

Thank you Lukas,

I really appreciate your prompt response and help.

Regards.

0 Kudos
Reply
5,046 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you use S32 Design Studio, open the startup_S32K144.S file and search for this section:

pastedImage_3.png 

Just modify the words as you need.

pastedImage_2.png

Regards,

Lukas

0 Kudos
Reply
5,046 Views
lohrsistemas
Contributor IV

Hi Lukas, thanks for your feedback.

I'm using IAR plugin, so, my startup_S32K144.S is a little diferent.

pastedImage_1.png

However, I need to protect the flash against reading, but I have to program and delete it normally via JTAG. My code is confidential, so, customers cant read.

To do this, how should I set the bits described in the print screen?

Thanks.

0 Kudos
Reply
5,046 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

In this case, change the FSEC byte. Default value is 0xFE which means the device is not secured (you can access everything via JTAG). Last two bits say if the device is secured or not:

pastedImage_1.png

Change the value from 0xFFFF7FFE to 0xFFFF7FFC or 0xFFFF7FFD or 0xFFFF7FFF and the device will be secured. You can enable backdoor key access if needed.

Regards,

Lukas