TWR-K60f120m and FRDM-K64f CAN communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60f120m and FRDM-K64f CAN communication

4,568 Views
smith1
Contributor II

I'm trying to setup CAN communication between the FRDM-K64f and the TWR-K60f120m with a TWR-SER board. I'm running the Flexcan example from the KSDK for the FRDM and the Flexcan example from MQX 4.2 for the TWR. I was wondering if there would be an issues hooking these two examples together? I know the MQX uses mailboxes from looking at the code, but I'm not sure if they will ruin the communication.

Labels (1)
0 Kudos
Reply
7 Replies

3,851 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Smith,

What do you mean " hooking these two examples together"?

if we need two CAN devices communicate, the two CAN interfaces must have same baud rate and can identify the correct ID.

the CAN demo under KSDK 2.0 package for FRDM-K64 is in loop-back mode. the exmaple sends a CAN Message from the Tx Message Buffer to the Rx Message Buffer throuth internal loopback interconnector in one device. We can not use it for two devices communication without modification.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,851 Views
smith1
Contributor II

by "hooking these two examples together", I meant using them together. And I set the enableLookback variable to false in the KSDK demo. Was there any other modifications besides that for two device communication?

And are there any jumper setting I need to change for the TWR-SER board? I hooked it up to see if I could pick anything up on an oscilloscope, but didn't get anything.

Thanks by the way.

0 Kudos
Reply

3,851 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

I just checked the schematic, TWR-SER has on board CAN transceiver but FRDM-K64 doesn't.

CAN point to point communication can work when both points have or haven't CAN transceiver.

But I highly suggest you have CAN transceiver for both sides completely match the CAN protocol. thus you need have a external CAN transceiver circuit for FRDM board.

after that, run program for each board. check if on chip CAN TX pin has signal when transmits, if no, check your code.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,851 Views
trialaccount12
Contributor V

Hi,

     I tried flexCAN example in FRDM k64F. Internal loop-back program was successful but when I run the interrupt mode method where I flashed flexCAN code in two FRDM k64F boards. One node being "a" and other being "b" as per the example.

   Connection wise I connected both TX together, Rx together and a common ground. I did not use CAN transreceiver with either of the boards. But it was not successful. Am i missing something here?

IDE: MCU xpresso.

Thanks and Regards

Niranjan

0 Kudos
Reply

3,851 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Niranjan,

This thread is from two years ago. we don't maintain it any more. Please create a new thread for your new question.

Appreciate your understanding.

Best Regards

Jennie Zhang

0 Kudos
Reply

3,851 Views
trialaccount12
Contributor V

HI,

    Thank you for the update. I have created a new thread:

https://community.nxp.com/thread/496759 

It would be helpful if you can take a look into it.

Thanks and Regards

Niranjan

0 Kudos
Reply

3,851 Views
trialaccount12
Contributor V

Hi,

   Pls ignore my previous post. I got it working. The issue was with Transreceivers. Thank you for your inputs.

Regards

Niranjan

0 Kudos
Reply