How we do Functional Testing of  PTP CARD(QorIQ P2020) with CODE WARRIER 

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How we do Functional Testing of  PTP CARD(QorIQ P2020) with CODE WARRIER 

1,126 Views
nareshpuli
Contributor III

 Functional Testing of  PTP CARD(QorIQ P2020) with CODE WARRIER  

 

1.VALIDATION OF ADT
2 VALIDATION OF INTERFACES (SERIAL & ETHERNET)
3 VALIDATION OF MEMORIES

 

How we do above testings of PTP with  codewarrior.

 

 

 

thanks & regards

Naresh

Labels (1)
0 Kudos
Reply
1 Reply

994 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello naresh puli,

If you want to use bareboard project, please download NetComm from NetComm Software Resources|NXP . Netcomm is a driver package for bare board project based on CodeWarrior. Since no use cases for P2020 platform in NetComm, you could refer to P1020 as an example, please use CodeWarrior to open use cases in NetCommSw\build\bare_1021_cw_build\UseCases\controller.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply