MPC8309 PTP IEEE 1588

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309 PTP IEEE 1588

2,435 Views
威杨
Contributor III

Hello,everyone

     I use MPC8309, i want to use ptp ieee 1588 as slave and master.but i find source code on http://sourceforge.net/projects/linuxptp/files/latest/download ,but the source code only support kernel of 3.xx or new.

but i want use it at 2.6.33.7. who can give me some advises?

0 Kudos
Reply
1 Reply

2,238 Views
Pavel
NXP Employee
NXP Employee

Use LTIB Linux BSP for the TWR-MPC8309 board. This BSP is available on the following page:

http://www.nxp.com/products/software-and-tools/hardware-development-tools/tower-development-boards/m...

See attached file.

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply