MPC5744p SIUL2 External Interrupt 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744p SIUL2 External Interrupt 0

3,085 Views
salahabbas
Contributor I

SIUL2 External Interrupt 0 trigerring:

 

does someone have an application example which uses the "SIUL2 External Interrupt 0" ?

 

i configured the MPC5744p to use the "SIUL2 External Interrupt 0" as an external input, and mapped the "ISRs 243" to my ISR243_Function(), and there are 2 huge problems:

 

1 => The interrupt never pens !  (Even the IVOR4 is never called !).

2=> Instead of that, i have an unexplained Reset (hapenning when setting the electrical line to HIGH state), and which makes my PC point to illegal memory area !!!

 

 

Your hel please !

 

Thank you so much.

 

Salah.

Labels (1)
0 Kudos
Reply
3 Replies

2,187 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

please check the example in the attachment.

Regards,

Martin

0 Kudos
Reply

2,187 Views
hangxie
Contributor III

Hi, martinkovar‌ , Can help for this issue? I have debug for days and the external interrupt all ways make the CPU reset.

0 Kudos
Reply

2,187 Views
hangxie
Contributor III

I have the same problem, the CPU reset when the external interrupt trig.

0 Kudos
Reply