pressure sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pressure sensor

1,894 Views
nourynoury
Contributor I

Hi i would like to use pressure sensor MPX2100A in my project

1-i read 110kpa what mean (atmosphic pressure +100 kpa )

2-is it possible to use arduino with this pressure sensor

Tags (1)
0 Kudos
1 Reply

1,683 Views
david_diaz
NXP Employee
NXP Employee

Hello Noury,

1. The MPX2100A is an absolute pressure sensor, which means that the device output refers to the absolute value of the force per-unit-area exerted on a surface. Therefore the absolute pressure is the difference between the pressure at a given point and the absolute zero of pressure or a perfect vacuum.

absolute.jpg

In this case you are not reading the atmospheric pressure, you are reading the pressure applied to P1.

2. Indeed, you can use the MPX2100A with the Arduino.

Please be aware that the MPX2100A is a compensated pressure sensor which means that the given output it’s already internally temperature compensated, so externally you only need to add the amplification circuit before sending the sensor’s signal to the MCU’s ADC.

You may refer to the following amplification circuit:

amplification.jpg

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!