IMX280 ./ltib ERR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX280 ./ltib ERR

Jump to solution
4,341 Views
tingning
Contributor II

look this

lxdialog/lxdialog.a(util.o): In function `draw_shadow':

util.c:(.text+0xa95): undefined reference to `has_colors'

util.c:(.text+0xacf): undefined reference to `wmove'

util.c:(.text+0xae4): undefined reference to `winch'

util.c:(.text+0xaf6): undefined reference to `waddch'

util.c:(.text+0xb26): undefined reference to `wmove'

util.c:(.text+0xb32): undefined reference to `winch'

util.c:(.text+0xb44): undefined reference to `waddch'

util.c:(.text+0xb50): undefined reference to `winch'

util.c:(.text+0xb62): undefined reference to `waddch'

util.c:(.text+0xb82): undefined reference to `wnoutrefresh'

collect2: ld returned 1 exit status

make: *** [mconf] Error 1

error: Bad exit status from /work/imx280/ltib/tmp/rpm-tmp.90388 (%build)

 

 

 

 

RPM build errors:

    Bad exit status from /work/imx280/ltib/tmp/rpm-tmp.90388 (%build)

Build time for lkc: 2 seconds

 

 

Failed building lkc

Died at ./ltib line 1392.

 

i don't know why that appear it

I do like this

1 down load ubuntu 12.04 and install

2 install arm-fsl-linux-gnueabi-gcc

3 down load  L2.6.35_1.1.0_130130_source.tar.gz  and install

4 install host packeages needed by LTIB,Execute this script

this script content:

#!/bin/bash
# Install packages needed by LTIB
sudo aptitude -y install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev
sudo aptitude -y install libdbus-glib-1-dev liborbit2-dev intltool
sudo aptitude -y install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool
sudo aptitude -y install uuid-dev liblzo2-dev
sudo aptitude -y install tcl dpkg
# Packages required for 64-bit Ubuntu
# Do "uname -a" and see if the word "x86_64" shows up.
if uname -a|grep -sq 'x86_64'; then
sudo aptitude -y install ia32-libs libc6-dev-i386 lib32z1
fi
# The following recommended for Linux development.
# They are not required by LTIB.
sudo aptitude -y install gparted emacs22-nox openssh-server
sudo aptitude -y install nfs-common nfs-kernel-server lintian
sudo aptitude -y install git-core git-doc git-email git-gui gitk
sudo aptitude -y install diffstat indent tofrodos fakeroot doxygen uboot-mkimage
sudo aptitude -y install sendmail mailutils meld atftpd sharutils
sudo aptitude -y install manpages-dev manpages-posix manpages-posix-dev linux-doc
sudo aptitude -y install vnc4server xvnc4viewer

5 ccache -M 50M  and ccache -c
annex is inmformation which printf log

Original Attachment has been moved to: host_config.log.zip

1 Solution
3,750 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ting ning,

I created am Ubuntu 12.04 Virtual Machine and tested installing LTIB. I was able to get very far with the patch on the following community document:

ubuntu-ltib-patch.tgz

However, I am now seeing a 404 error for lkc. There missing package is available on the following document:

Using i.MX 6 Series LTIB on Host Ubuntu 14.04 Trusty Tahr

I will try it, in the meantime I hope it helps!

View solution in original post

4 Replies
3,750 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ting Ning,

This error is similar to the one described in the following thread:

Re: LTIB build fails on lkc, using Ubuntu 11.10 and LTIB 9.1.1

Would you try it and let us know if it helps? LTIB was tested with older Ubuntu versions so some packages may give a bit of trouble in 12.04.

0 Kudos
Reply
3,750 Views
tingning
Contributor II

The situation is getting worse,I install  519-oneiricltibpatch.tgz and ./install-patches.sh and  rm -rf /opt/*

./ltib

it have not anyting  is created in opt directory

0 Kudos
Reply
3,751 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ting ning,

I created am Ubuntu 12.04 Virtual Machine and tested installing LTIB. I was able to get very far with the patch on the following community document:

ubuntu-ltib-patch.tgz

However, I am now seeing a 404 error for lkc. There missing package is available on the following document:

Using i.MX 6 Series LTIB on Host Ubuntu 14.04 Trusty Tahr

I will try it, in the meantime I hope it helps!

3,750 Views
tingning
Contributor II

Hello gusarambula,

Thank you for help me

You let me know method

:smileycool:The ic very mature and a lots of Datasheet.

Now  i  have  been able to configure the kernel

Thanks again!!!