i.MX6SoloX RGMII1_TX_CTL delay to AR8035

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SoloX RGMII1_TX_CTL delay to AR8035

3,326 Views
christianpeters
Contributor I

Hi Community,

according to the datasheet of the AR8035 the RGMII1_TX_CTL has to be delayed from . 1.5 to 2ns.

The iMX6SoloX cannot do this. and the integrated delay of the AR8035 is too long with 2,4 nS.

It is not feasible to get the delay by making the track long enough.

Is there easy way to produce the necessary delay?

Thanks a lot.

Christian Peters FAE EBV

Labels (1)
0 Kudos
Reply
5 Replies

2,721 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6SX Datasheet(s) recommend hardware delay (of greater than 1.5 ns and less than 2.0 ns)
for the  clock signal. This may be implemented as PCB trace delay or delay scheme. Basically

RGMII specs allow implementation of a delay on TXC or RXC inside the transmitter, but - as we
see -
this delay option is not configurable neither for i.MX6SX ENET nor the external PHY.
The Datasheet
recommends PCB trace solution.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,721 Views
christianpeters
Contributor I

Dear Yuri,

a pcb trace solution would mean a 260mm trace @ 1,75 nS.

This from layout and EMV point of view, very poor and not feasible.

Any other recommendations?

Thanks for your help.

Christian

0 Kudos
Reply

2,721 Views
Yuri
NXP Employee
NXP Employee

circuit-board-traces.jpg

Just as an example of implementation

~Yuri.

0 Kudos
Reply

2,721 Views
christianpeters
Contributor I

Hi Juri,

this does not really help as the parts a ECL technology and start at 5$ upwards..

How do NXP realize the delay on the reference board ?

Christian

0 Kudos
Reply

2,721 Views
Yuri
NXP Employee
NXP Employee

  The following is i.MX6SX refrence design Summary page :

SABRE Board Reference Design|NXP

Regards,

Yuri.

0 Kudos
Reply