MK10FN1M0VLQ12: Use the internal band gap voltage for ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10FN1M0VLQ12: Use the internal band gap voltage for ADC

3,784 Views
markosiponen
Contributor III

I want to use the internal bandgap voltage as a reference voltage for the internal ADC.

I activate the band gap like this:

    VREF->SC = VREF_SC_VREFEN_MASK | VREF_SC_REGEN_MASK | VREF_SC_MODE_LV(2);

  

    while ((VREF->SC & VREF_SC_VREFST_MASK) == 0); // Wait for the bandgap ref to activate

I use VREF_SC_MODE_LV(2) because my debugger (KEIL) says that 2 = Tight regulation buffer enabled.

0 = Bandgap on only, for stabilization and startup

1 = Reserved

2 = Tight regulation buffer enabled

3 = Reserved

But the reference manual says:

00 Bandgap on only, for stabilization and startup

01 High-power buffer enabled

10 Reserved

11 Reserved

It does not work if i select VREF_SC_MODE_LV(1) , only if I use VREF_SC_MODE_LV(2) . But I can't find this information in any datasheet or reference manual? Where can I find this? Where did KEIL find this conflicting information?

And does the ADC use the buffered reference voltage or the Bandgap voltage?

And one more thing. The reference manual says the band gap voltage is 1.2V but the data sheet says 1.195V. Which is correct?

And finally one more thing. When I measure pin 37 (VREF_OUT) I get 0 V. Do I need to enable the pin? I have tried both VREF_SC_MODE_LV(1) and VREF_SC_MODE_LV(2) with no luck.

Tags (1)
0 Kudos
Reply
1 Reply

3,271 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hello markosiponen

You need set the VREF bit in SIM_SCGC4 first , then configure VREF->SC.

Q1:Does the ADC use the buffered reference voltage or the Bandgap voltage?

A1:The PMC bandgap 1V reference voltage is one of the input signal for ADC.  The 1.195V buffered reference voltage is one of the voltage reference source for ADC.

Q2:The reference manual says the band gap voltage is 1.2V but the data sheet says 1.195V. Which is correct?

A2:Data sheet is correct. For more detail you can see the "Table 36. VREF full-range operating behaviors" in the Data sheet (K10P144M120SF3.pdf) .

Best Regards

Robin

0 Kudos
Reply