Error in Input Curent Calibration of WCT 5WTXAUTO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in Input Curent Calibration of WCT 5WTXAUTO

Jump to solution
1,878 Views
santoshpulasani
Contributor III

Hi,

 

Following the instructions from

WCT 1001A/WCT1003A Run -Time  Debugging User’s Guide ,Tried to do the Input Curent Calibration of WCT 5WTXAUTO But the board after entering into debug mode does not allow for the receiver to get power.i.e no power at receiver.

 

So unable to change diffferent load currents as per the sujjestion in the above document.

 

 

Looking for help in regard to Input Current Calibration of WCT 5WTXAUTO.

 

can any one sujjest a way.

 

Best Regards,

Santosh Reddy Pulasani

Labels (1)
1 Solution
1,666 Views
Stano
NXP Employee
NXP Employee

Hi Santosh,

You can make the basic calibration of the A13 demo board in "Debug" mode. You will need the standard multimeter for the input voltage, input current and Characterization parameters calibration. For the last calibration step you need to use the AVID Qi FOD Receiver.

The detail description of the whole calibration process is in this document:

http://cache.nxp.com/files/microcontrollers/doc/user_guide/WCT100XARTDUG.pdf?fpsp=1&WT_TYPE=Users%20...

The all other usable documents are on this page:

5W Wireless Charging Transmitter ICs|NXP

Best Regards,

Stano.

View solution in original post

2 Replies
1,667 Views
Stano
NXP Employee
NXP Employee

Hi Santosh,

You can make the basic calibration of the A13 demo board in "Debug" mode. You will need the standard multimeter for the input voltage, input current and Characterization parameters calibration. For the last calibration step you need to use the AVID Qi FOD Receiver.

The detail description of the whole calibration process is in this document:

http://cache.nxp.com/files/microcontrollers/doc/user_guide/WCT100XARTDUG.pdf?fpsp=1&WT_TYPE=Users%20...

The all other usable documents are on this page:

5W Wireless Charging Transmitter ICs|NXP

Best Regards,

Stano.

1,666 Views
santoshpulasani
Contributor III

Hi Stano,

Appreciate you Sujjestion.

The Input Current calibration worked.

Thank You.:smileyhappy:

Best Regards,

Santosh

0 Kudos
Reply