About S912XET256 maskset firmware Rev.A and Rev.B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About S912XET256 maskset firmware Rev.A and Rev.B

2,086 Views
Alan_AVN
Contributor I

Hi,

According to MC9S12XEP100RM, it mentions that S912XET256 maskset provides two firmware - Rev.A and Rev.B. But, reference manual doest not explain their difference. Someone who can tell me their difference? Thanks a lot!

 

Alan

116486_116486.pngpastedImage_3.png

Labels (1)
0 Kudos
Reply
1 Reply

1,736 Views
RadekS
NXP Employee
NXP Employee

Hi Alan,

In case of S12XET256

Rev.A means maskset 1M53J or 0N36H

Rev.B means maskset 2M53J or 1N36H.

So, RevB is newer version of maskset without specification of manufacturing Fab Site.

Note: Masksets M53J are produced in TSMC FAB3

Note: Masksets N36H are produced in TSMC11

According compare 1M53J and 2M53J maskset errata, maskset 2M53J have fixed several bugs in Emulated EEPROM firmware.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply