i.MX6SDL HDMI CEC and DCD.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL HDMI CEC and DCD.

1,875 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL HDMI CEC.

Actually, they have some troubles to use HDMI CEC and DCD.

Then, they want to know the effect between CEC and DCD each other.

Can they use HDMI CEC (DCD) even if they have a DCD (CEC) trouble?

Or in order to use one of the above, they must resolve the other problem?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

1,595 Views
gusarambula
NXP TechSupport
NXP TechSupport

There is some information that may help, unfortunately it is moderated so an NDA is required. This thread is being handled trough a SR. (1-3744532874)