IMX53 Loco based board with MT29F8G08ABABA as NFC 8bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 Loco based board with MT29F8G08ABABA as NFC 8bit

2,485 Views
cristiansicilia
Contributor III

Hello *,

we have a IMX53 board, based on LOCO, but we adding the MT29F8G08ABABA NAND using NANDF_D[7:0], CS0, WP_B#.

Booting with kernel it work good, infact I use the NAND as rootfs, I have also write a uImage kernel in a partition in 0x1000000 position, but when I load it in u-boot I obtain:

MR&D NSIP Feb  9 2015 18:48:13> nand read 0x70800000 0x1000000 0x8000

NAND read: device 0 offset 0x1000000, size 0x8000

32768 bytes read: OK

MR&D NSIP Feb  9 2015 18:48:13> md.b 0x70800000 0x10

70800000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................

...

I can't read (I'm sure that in this location there is a Kernel image) obtain only 0xFF for all data.

I can't also write:

MR&D NSIP Feb  9 2015 18:25:49> nand erase 0x0 0x80000

NAND erase: device 0 offset 0x0, size 0x80000

nand0: MTD Erase failure: -5

OK

In the board file, we setup nfc:

#ifdef CONFIG_MXC_NAND

void setup_nfc(void)

{

  u32 i, reg;

  u32 cfg = (PAD_CTL_PKE_ENABLE | PAD_CTL_PUE_PULL |

  PAD_CTL_100K_PU | PAD_CTL_ODE_OPENDRAIN_NONE |

  PAD_CTL_DRV_HIGH);

  #define M4IF_GENP_WEIM_MM_MASK          0x00000001

  #define WEIM_GCR2_MUX16_BYP_GRANT_MASK  0x00001000

  reg = __raw_readl(M4IF_BASE_ADDR + 0xc);

// reg &= ~M4IF_GENP_WEIM_MM_MASK;

    reg |= M4IF_GENP_WEIM_MM_MASK;          //NANDF on PATA_DATA

  __raw_writel(reg, M4IF_BASE_ADDR + 0xc);

// for (i = 0x4; i < 0x94; i += 0x18) {

// reg = __raw_readl(WEIM_BASE_ADDR + i);

// reg &= ~WEIM_GCR2_MUX16_BYP_GRANT_MASK;

// __raw_writel(reg, WEIM_BASE_ADDR + i);

// }

  /* To be compatible with some old NAND flash,

  * limit NFC clocks as 34MHZ. The user can modify

  * it according to dedicate NAND flash

  */

  clk_config(0, 34, NFC_CLK);

  mxc_request_iomux(MX53_PIN_NANDF_CS0,

  IOMUX_CONFIG_ALT0);

  mxc_iomux_set_pad(MX53_PIN_NANDF_CS0, cfg | PAD_CTL_HYS_ENABLE);

// mxc_request_iomux(MX53_PIN_NANDF_CS1,

// IOMUX_CONFIG_ALT0);

// mxc_iomux_set_pad(MX53_PIN_NANDF_CS1,

// PAD_CTL_DRV_HIGH);

// mxc_request_iomux(MX53_PIN_NANDF_CS2,

// IOMUX_CONFIG_ALT0);

// mxc_iomux_set_pad(MX53_PIN_NANDF_CS2,

// PAD_CTL_DRV_HIGH);

// mxc_request_iomux(MX53_PIN_NANDF_CS3,

// IOMUX_CONFIG_ALT0);

// mxc_iomux_set_pad(MX53_PIN_NANDF_CS3,

// PAD_CTL_DRV_HIGH);

  mxc_request_iomux(MX53_PIN_NANDF_RB0,

  IOMUX_CONFIG_ALT0);

  mxc_iomux_set_pad(MX53_PIN_NANDF_RB0, cfg | PAD_CTL_HYS_ENABLE);

  mxc_request_iomux(MX53_PIN_NANDF_CLE,

  IOMUX_CONFIG_ALT0);

  mxc_iomux_set_pad(MX53_PIN_NANDF_CLE, cfg | PAD_CTL_HYS_ENABLE);

  mxc_request_iomux(MX53_PIN_NANDF_ALE,

  IOMUX_CONFIG_ALT0);

  mxc_iomux_set_pad(MX53_PIN_NANDF_ALE, cfg | PAD_CTL_HYS_ENABLE);

  //gpio6->9 | WP#0  Write Protect

  mxc_request_iomux(MX53_PIN_NANDF_WP_B,

  IOMUX_CONFIG_ALT0);

// reg = readl(GPIO6_BASE_ADDR + GPIO_GDIR);

// reg |= 0x200;

// writel(reg, GPIO6_BASE_ADDR + GPIO_GDIR);

//

// reg = readl(GPIO6_BASE_ADDR + GPIO_DR);

// reg |= 0x200;

// writel(reg, GPIO6_BASE_ADDR + GPIO_DR);

  mxc_iomux_set_pad(MX53_PIN_NANDF_WP_B, cfg | PAD_CTL_HYS_ENABLE);

  mxc_request_iomux(MX53_PIN_NANDF_RE_B,

  IOMUX_CONFIG_ALT0);

  mxc_iomux_set_pad(MX53_PIN_NANDF_RE_B, cfg | PAD_CTL_HYS_ENABLE);

  mxc_request_iomux(MX53_PIN_NANDF_WE_B,

  IOMUX_CONFIG_ALT0);

  mxc_iomux_set_pad(MX53_PIN_NANDF_WE_B, cfg | PAD_CTL_HYS_ENABLE);

  mxc_request_iomux(MX53_PIN_ATA_DATA0,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA0, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA1,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA1, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA2,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA2, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA3,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA3, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA4,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA4, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA5,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA5, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA6,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA6, cfg);

  mxc_request_iomux(MX53_PIN_ATA_DATA7,

  IOMUX_CONFIG_ALT3);

  mxc_iomux_set_pad(MX53_PIN_ATA_DATA7, cfg);

}

#endif

In the Identification file ndand_ids.c we add:

,

    {"ONFI NAND 3,3V 8-bit", 0x38, 0, 1024, 0, LP_OPTIONS },

,..

In nand_device_info.c we add

,

    {

  .end_of_table             = false,

  .manufacturer_code        = 0x2c,

  .device_code              = 0x38,

  .cell_technology          = NAND_DEVICE_CELL_TECH_SLC,

  .chip_size_in_bytes       = 1LL*SZ_1G,

  .block_size_in_pages      = 128,

  .page_total_size_in_bytes = 4*SZ_1K + 224,

  .ecc_strength_in_bits     = 16,

  .ecc_size_in_bytes        = 512, //540,

  .data_setup_in_ns         = 25,

  .data_hold_in_ns          = 15,

  .address_setup_in_ns      = 10,

  .gpmi_sample_delay_in_ns  = 6,

  .tREA_in_ns               = -1,

  .tRLOH_in_ns              = -1,

  .tRHOH_in_ns              = -1,

  "MT29F8G08ABABA",

  },

  {true}

In board file header, we add:

//#define CONFIG_MTD_DEBUG

#define CONFIG_MTD_DEBUG_VERBOSE 1000

#define CONFIG_CMD_MTDPARTS

#define CONFIG_JFFS2_CMDLINE

#define CONFIG_MTD_DEVICE

#define CONFIG_MTD_PARTITIONS

#define MTDIDS_DEFAULT "nand0=nand0"

//#define MTDPARTS_DEFAULT "mtdparts=nand0:0xc00000@0x0(bootloader),0x400000@0xc00000(factory.id),0x500000@0x1000000(nand.kernel),10000000@0x1500000(nand.rootfs),0x10000000@0x11500000(nand.app),-@0x21500000(nand.rwfs)"

#define MTDPARTS_DEFAULT "mtdparts=nand0:0xc00000@0x0(bootloader),0x400000@0xc00000(factory.id),0x500000@0x1000000(nand.kernel),-@0x1500000(nand.all)\0"

#define MTD_ACTIVE_PART "nand0,1"

/* Enable below configure when supporting nand */

#define PPCHAMELON_NAND_TIMER_HACK

#define CONFIG_CMD_NAND

#define CONFIG_MXC_NAND

#define CONFIG_CMD_NAND_LOCK_UNLOCK

#define CONFIG_SYS_NAND_PAGE_4K

/* NAND FLASH driver setup */

#define CONFIG_SYS_NAND_MAX_CHIPS     8

#define CONFIG_SYS_MAX_NAND_DEVICE    1

#define CONFIG_SYS_NAND_BASE          0x40000000

#define CONFIG_NAND_FW_16BIT    0 /* 1: 16bit 0: 8bit */

#define CONFIG_CMD_NAND_LOCK_UNLOCK

#define CONFIG_SYS_NAND_ONFI_DETECTION

#define CONFIG_SYS_NAND_CSOR   (CSOR_NAND_ECC_ENC_EN   /* ECC on encode */ \

                               | CSOR_NAND_ECC_DEC_EN  /* ECC on decode */ \

                               | CSOR_NAND_ECC_MODE_4  /* 4-bit ECC */ \

                               | CSOR_NAND_RAL_3       /* RAL = 3Byes */ \

                               | CSOR_NAND_PGS_4K      /* Page Size = 4K */ \

                               | CSOR_NAND_SPRZ_224    /* Spare size = 224 */ \

                               | CSOR_NAND_PB(128))  /*Pages Per Block = 128 */

#define CONFIG_SYS_NAND_BLOCK_SIZE     (512 * 1024)

#define CONFIG_SYS_NAND_BASE_LIST      { CONFIG_SYS_NAND_BASE }

#define CONFIG_SYS_MAX_NAND_DEVICE     1

//#define CONFIG_MTD_NAND_VERIFY_WRITE

#define CONFIG_CMD_FLASH

#define CONFIG_SYS_NAND_FTIM0  (FTIM0_NAND_TCCST(0x07)| \

                                       FTIM0_NAND_TWP(0x18)   | \

                                       FTIM0_NAND_TWCHT(0x07) | \

                                       FTIM0_NAND_TWH(0x0a))

#define CONFIG_SYS_NAND_FTIM1  (FTIM1_NAND_TADLE(0x32)| \

                                       FTIM1_NAND_TWBE(0x39)  | \

                                       FTIM1_NAND_TRR(0x0e)   | \

                                       FTIM1_NAND_TRP(0x18))

#define CONFIG_SYS_NAND_FTIM2  (FTIM2_NAND_TRAD(0x0f) | \

                                       FTIM2_NAND_TREH(0x0a)  | \

                                       FTIM2_NAND_TWHRE(0x1e))

#define CONFIG_SYS_NAND_FTIM3  0x0

Labels (2)
Tags (3)
0 Kudos
Reply
2 Replies

1,912 Views
b36401
NXP Employee
NXP Employee

Please refer these resources regarding adding new NAND:  

1.

https://community.freescale.com/message/295870#295870

2.

Section 7.4.4 (NAND Flash Driver and Commands) of AN4173

http://cache.freescale.com/files/dsp/doc/app_note/AN4173.pdf 

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,912 Views
cristiansicilia
Contributor III

Hello,

I re-check the implementation, but I don't understand the problem.

My suspect is that the basic driver need some fix for this nand, I also tried

.page_total_size_in_bytes = 4*SZ_1K + 218,

but the problem remain, seems a fake read and a fake write...

Anyone use this NAND with U-BOOT?

0 Kudos
Reply