Booting T1040RDB 64-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting T1040RDB 64-bit

Jump to solution
4,053 Views
jaket
Contributor II

Hi, I am trying to boot the T1040RDB in 64-bit mode and am encountering a problem.

First, I configured a yocto environment for 64-bit "fsl-setup-poky t1040rdb-64b" and built my images.

Next, I'm trying to do a tftp boot using the exact same method I can use successfully with the 32-bit build but with the 64-bit images instead. The steps are described in section 11.2 of the QorIQ T1040 RDB Quick start. Basically, I load my 64-bit uImage into 0x1000000, the rootfs into 0x200000 and the dtb into 0xc00000 and finally do a bootm.

After I run boot I get the following console output with the error on the final line:

Bytes transferred = 5103719 (4de067 hex)

WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-3.12.19-rt30-QorIQ-SDK-V1.

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    5103655 Bytes = 4.9 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 02000000 ...

   Image Name:   fsl-image-minimal-t1040rdb-64b-2

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    3308708 Bytes = 3.2 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 00c00000

   Booting using the fdt blob at 0xc00000

   Uncompressing Kernel Image ... OK

   Loading Ramdisk to 2fcd8000, end 2ffffca4 ... OK

ERROR: image is not a fdt - must RESET the board to recover.

If I just tftp over the dtb file to 0xc00000 and examine it using the fdt command from u-boot everything looks fine.

=> run my_dtb

=> fdt addr 0xc00000

=> fdt header

magic:                  0xd00dfeed

totalsize:              0x8b47 (35655)

off_dt_struct:          0x38

off_dt_strings:         0x7ff0

off_mem_rsvmap:         0x28

version:                17

last_comp_version:      16

boot_cpuid_phys:        0x0

size_dt_strings:        0x757

size_dt_struct:         0x7fb8

number mem_rsv:         0x0

Any ideas what is going on? Is it okay that u-boot is in 36 bit addressing mode or do I need to rebuild part of the flash?

Thanks, Jake

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,993 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello  Jacob Tummond,


U-boot decompresses Linux Kernel image to lower address. The 64bit uImage size is larger than 32 bit uImage, dtb file is overwritten by the uncompressed Kernel image, you could use the following addresses to deploy images.

tftp 1000000 $dir/$bootfile;tftp 4000000 $dir/$ramdiskfile;tftp e00000 $dir/$fdtfile;setenv bootargs root=/dev/ram rw console=ttyS0,115200 $othbootargs;
bootm 1000000 4000000 e00000


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,994 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello  Jacob Tummond,


U-boot decompresses Linux Kernel image to lower address. The 64bit uImage size is larger than 32 bit uImage, dtb file is overwritten by the uncompressed Kernel image, you could use the following addresses to deploy images.

tftp 1000000 $dir/$bootfile;tftp 4000000 $dir/$ramdiskfile;tftp e00000 $dir/$fdtfile;setenv bootargs root=/dev/ram rw console=ttyS0,115200 $othbootargs;
bootm 1000000 4000000 e00000


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,993 Views
jaket
Contributor II

That did the trick! Thanks, Jake

0 Kudos
Reply