I have compiled and uploaded the Freescale 4.1.1 virtual_nic example - how do I verify it is working?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have compiled and uploaded the Freescale 4.1.1 virtual_nic example - how do I verify it is working?

3,435 Views
rickstuart
Contributor V

Hi all,

[What I really want is to open a discussion on the virtual_nic Freescale example to understand it better.  But in other forums I find it more effective to ask one specific per thread.  Please let me know if that is not the culture here.]

I have compiled and uploaded the Freescale 4.1.1 virtual_nic example to a Tower w/a K70.  I am working with IAR Workbench.  How do I verify it is working?

I have read somewhere that this example only implements one direction of the Ethernet-over-USB to Ethernet connection. If so, I am at a loss to think of a good test for this example.  Further, inspecting the code, it looks symmetrical.  That is, I believe I see code for transmitting in both directions (USB port and RJ45 port).

In another post/thread, a Freescale employee said I should be able to PING the connection.  I tried this but apparently it did not work.

-thank you

5 Replies

2,849 Views
rickstuart
Contributor V

Success, I have been able to ping this example.  But only after I change the IP address found in virtual_nic_enet.h.  If I don't change it to match the subnet of the network I plug the RS45 into, the ping does not work.  Further, when I am using the default IP address and I look at the output of "route print", I see values that come close but DO NOT MATCH the default IP address found in virtual_nic_enet.h.

Maybe to some this is just plain Windows-networking-101.  But to me it is darn confusing - and  I would really appreciate it if someone could set me straight.

For instance, if this example is truly only a Ethernet gate way between the USB world and the RJ45 world - then why is there even the need for an IP address?

-thanks

0 Kudos
Reply

2,849 Views
rickstuart
Contributor V

I take that back.  No success here.   I am trying to duplicate Freescale employee's Martin comment that he plugged a router into the TWR-SER RJ45.  But that does not create the expected network (It does create a new network but the expected routing is missing).  As a GOLD test I used a off-the-shelf TRENDNET Ethernet over USB to Ethernet 10/100BaseT converter dongle in place of the Freescale TWR running the Freescale CDC Ethernet over USB example.  That worked with the router.  It created a network and the Win7 box connected through the router's WIFI to the local network.  I repeated this GOLD test successfully using Ubuntu and all the same hardware (same Win7 box, TRENDNET & ASUS router).

Any pointers getting this Freescale running like the TRENDNET dongle would be appreciated.

-thanks

0 Kudos
Reply

2,849 Views
rickstuart
Contributor V

Tidying up this thread...

I think the Freescale virtual_nic CDC Example has a problem in the USB to Ethenet direction.  I explain what I did here in this thread:

USB Virtual NIC

I'm not sure my solution is a good one.  But I can ARP and Ping now using my modified virtual_nic code.

2,849 Views
RadekS
NXP Employee
NXP Employee

Thank you for your bug report.

It was reported to our internal bug database and it will be fixed in one of next MQX releases.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,849 Views
rickstuart
Contributor V

I think I found the problem.  In file "virtual_nic_enet.c" in "fuction VNIC_FEC_Send()"  if you change this code:

USB_mem_copy(ethernet_frame_ptr + 2 * MAC_ADDR_SIZE,
   g_enet_hdr.TYPE, 2);
protocol = *((uint16_t *)(((ENET_HEADER_PTR)ethernet_frame_ptr)->TYPE));
nic_pcb = _mem_alloc_system_zero(sizeof(PCB) + sizeof(PCB_FRAGMENT));
if(nic_pcb == NULL)

...to this...

USB_mem_copy(ethernet_frame_ptr + 2 * MAC_ADDR_SIZE,
   g_enet_hdr.TYPE, 2);
protocol = *((uint16_t *)(((ENET_HEADER_PTR)ethernet_frame_ptr)->TYPE));
protocol = htons(protocol);
nic_pcb = _mem_alloc_system_zero(sizeof(PCB) + sizeof(PCB_FRAGMENT));
if(nic_pcb == NULL)

The Type field sent out the RJ45 side will work for ARP & Ping.  It appears to work for other message but I wasn't testing for them specifically.

-thanks

0 Kudos
Reply