i.mx6 with GPS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 with GPS

2,130 Views
sergkot
Contributor II

Hello,

I'm having a problem with GPS (originGPS ORG1410) on my board. I determined that i.mx6 board (may be ddr memory) creates electromagnetic interference on the GPS module, that why GPS module can not find the coordinates.

Does somebody have the same problem?


Thanks in advance for all of the help!

Serg

Labels (1)
0 Kudos
Reply
1 Reply

1,620 Views
igorpadykov
NXP Employee
NXP Employee

Hi sergkot

this is more design/shielding problem. Seems for complete

solution one can look for example below, 8.17 GPS module

Linux Software User Manual (i.MX6) - BlueWiki

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply