I am going to test the DPAA driver for t1040,but I am new to this driver,so anyone can suggest me some test cases or test scenarios for testing the DPAA driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am going to test the DPAA driver for t1040,but I am new to this driver,so anyone can suggest me some test cases or test scenarios for testing the DPAA driver

3,114 Views
syamadas
Contributor I

I am going to test the DPAA driver for t1040,but I am new to this driver,so anyone can suggest me some test cases or test scenarios for testing the DPAA driver

0 Kudos
Reply
4 Replies

2,519 Views
aravindganesan
Contributor I

Hello syama Das,

Which driver you want to test?

DPAA contains SEC,PME,SRIO and so on.

U please refer the manual

Freescale Technical Information Center

->linux user space->usdpaa applications

Thanks,

Aravind Ganesan

0 Kudos
Reply

2,519 Views
syamadas
Contributor I

Hi Aravind,

I wanted to test the FMan,QMan and BMan are working as expected or not. And mostly I want test some functionality of   Linux Ethernet Driver for DPAA(like Private DPAA Ethernet Driver,Shared DPAA Ethernet Driver etc.).If you suggest me some scenarios for SEC and PME also that will be great.

0 Kudos
Reply

2,519 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Syama,

In the Section "Benchmark Reproducibility Guides" contains some test scenarios, for example IP Forward, IPSEC, Netperf, etc. USDPAA also provides some applications, for example reflector, IPForward, etc.

About the shared MAC technology, there are two methods, a MAC device is shared between different partitions under a Hypervisor and second a MAC device is shared between USDPAA and Linux Kernel.

I think probably you are interested in the second one. Under USDPAA document "Freescale P4080/P5020/P3041 USDPAA IPFwd Longest Prefix Match User Manual" contains a section "How to run shared MAC interface", you could have a reference. Here you could use other USDPAA application (for example reflector) to do verification.

USDPAA also provides some applications for PME and IPSecfwd.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,519 Views
lunminliang
NXP Employee
NXP Employee

Yes, please use the latest version SDK1.6 which introduce T1040 as a new device supported.

0 Kudos
Reply