Nitrogen6x and SATA HD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nitrogen6x and SATA HD

Jump to solution
5,320 Views
gonfer
Contributor V

Hi all,

I've just plugged a SATA-HD to my new Nitrogen6x board and it looks U-Boot detects fine the HD but linux doesn't.

This is an excerpt of the console output from U-Boot:

_____________________________________________________________________________

U-Boot 2014.04-00119-g8a29f55 (Apr 25 2014 - 11:00:09)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

Reset cause: POR

Board: Nitrogen6X

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB

*** Warning - bad CRC, using default environment

No panel detected: default to HDMI

Display: HDMI (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   using phy at 6

FEC [PRIME], usb_ether

Hit any key to stop autoboot:  0

AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode

flags: ncq stag pm led clo only pmp pio slum part

SATA Device Info:

S/N:         K11ET7325C46

Product model number: FUJITSU MHW2080BH

Firmware version: 0000001C

Capacity: 156301488 sectors

SATA device 0: Model: FUJITSU MHW2080BH Firm: 0000001C Ser#:         K11ET7325C46

            Type: Hard Disk

            Supports 48-bit addressing

            Capacity: 76319.0 MB = 74.5 GB (156301488 x 512)

... is now current device

** Unrecognized filesystem type **

Failed to mount ext2 filesystem...

** Unrecognized filesystem type **

SATA device 1: unknown device

** Bad device sata 1 **

_____________________________________________________________________________

Linux boots fine, but the only mention to "sata" in dmesg is:

No sata disk.

Everything is just out of the box; I'm just running the SD that comes with the board.

U-Boot > version

U-Boot 2014.04-00119-g8a29f55 (Apr 25 2014 - 11:00:09)

arm-linux-gnueabihf-gcc (Ubuntu/Linaro 4.8.2-16ubuntu4) 4.8.2

GNU ld (GNU Binutils for Ubuntu) 2.24

# uname -a

Linux nitrogen6x 3.0.35-ts-armv7l #1 SMP PREEMPT Thu Aug 8 14:44:15 EDT 2013 armv7l GNU/Linux

My question is, does this kernel have SATA support enabled?

Regards,

Gonzalo.

Tags (3)
0 Kudos
Reply
1 Solution
4,134 Views
tonyzheng
NXP Employee
NXP Employee

Hello.

As far as I know, linux 3.0.35 for imx6q Sabre SDP well supports SATA HD, but it needs a patch to fix some SATA recognition bugs. I don't konw whether your board have updated it.


View solution in original post

0 Kudos
Reply
12 Replies
4,135 Views
tonyzheng
NXP Employee
NXP Employee

Hello.

As far as I know, linux 3.0.35 for imx6q Sabre SDP well supports SATA HD, but it needs a patch to fix some SATA recognition bugs. I don't konw whether your board have updated it.


0 Kudos
Reply
4,134 Views
EricNelson
Senior Contributor II

Hello Tao,

Do you have a specific reference to patches?

0 Kudos
Reply
4,134 Views
tonyzheng
NXP Employee
NXP Employee

Hi,

The attachment is the patch for imx6q sabresd SATA link problems.( Linux 3.0.35)

0 Kudos
Reply
4,134 Views
EricNelson
Senior Contributor II

Many thanks, Tao!

0 Kudos
Reply
4,134 Views
tonyzheng
NXP Employee
NXP Employee

It's my pleasure!

0 Kudos
Reply
4,134 Views
gonfer
Contributor V

Hi Tao,

thanks for pointing that - I didn't know about that SATA recognition bug.

So I've come back to Boundary's website and have found this image: yocto-3.10.17-beta-20140303.img.gz

I've burned it in a new SD and now it looks ok:

- U-Boot detects the HD:

     AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode

     flags: ncq stag pm led clo only pmp pio slum part

     SATA Device Info:

     S/N:         K11ET7325C46

     Product model number: FUJITSU MHW2080BH

     Firmware version: 0000001C

     Capacity: 156301488 sectors

     SATA device 0: Model: FUJITSU MHW2080BH Firm: 0000001C Ser#:         K11ET7325C46

                 Type: Hard Disk

                 Supports 48-bit addressing

                 Capacity: 76319.0 MB = 74.5 GB (156301488 x 512)

     ... is now current device

- Linux detects the HD:

     ahci: SSS flag set, parallel bus scan disabled

     ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode

     ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst

     scsi0 : ahci_platform

     ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71

and /dev/sda is present.

root@nitrogen6x:~# uname -a

Linux nitrogen6x 3.10.173.10.17_beta+yocto+g9260843 #1 SMP Sun Mar 2 15:16:18 MST 2014 armv7l GNU/Linux

That's enough for me. I can continue evaluating the processor and board capabilities.

Thanks sooooo much !!!

Gonzalo.

0 Kudos
Reply
4,134 Views
EricNelson
Senior Contributor II

Hi Gonzalo,

The cards we ship with Nitrogen6x should absolutely support SATA out of the box (including booting to SATA).

The kernel messages related to SATA are normally prefixed with ahci:

ahci: SSS flag set, parallel bus scan disabled

ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode

ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst

scsi0 : ahci_platform

ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02200fff] port 0x100 irq 71

If things are working, you should see devices named "/dev/sda*". From the messages above, it appears that you haven't yet partitioned the drive, so nothing will try to mount.

0 Kudos
Reply
4,134 Views
gonfer
Contributor V

Thanks for your answer, Eric.

I don't see any kernel message as in your post; only No sata disk, and /dev/sda is not present in my system.

I'm not sure what's going on, as it looks U-Boot detects correctly the HD. Do you have any clue about what to look for? Just try a different HD?

Gonzalo.

0 Kudos
Reply
4,134 Views
EricNelson
Senior Contributor II

There's no indication that the hard drive is a problem, since U-Boot sees it.

Can you double-check the kernel configuration?

# zcat /proc/config.gz | grep AHCI

CONFIG_IMX_HAVE_PLATFORM_AHCI=y

# CONFIG_SATA_AHCI is not set

CONFIG_SATA_AHCI_PLATFORM=y

# CONFIG_SATA_ACARD_AHCI is not set

0 Kudos
Reply
4,134 Views
gonfer
Contributor V

My kernel configuration matches yours:

# zcat /proc/config.gz | grep AHCI

CONFIG_IMX_HAVE_PLATFORM_AHCI=y

# CONFIG_SATA_AHCI is not set

CONFIG_SATA_AHCI_PLATFORM=y

# CONFIG_SATA_ACARD_AHCI is not set

0 Kudos
Reply
4,134 Views
EricNelson
Senior Contributor II

Hi Gonzalo,

I'm confused by the kernel version shown above. We ship kernels built out of a git tree which have a direct git reference (in "uname" or /proc/version).

Is this an SD card image that you got from Timesys? All of theirs should also have SATA support, but something is clearly wrong, and it seems to be kernel related, even though your CONFIG settings above look right.

Can you run a quick test against this image?

     http://boundarydevices.com/yocto-dora-release-mx6/

Please advise,


Eric

0 Kudos
Reply
4,134 Views
gonfer
Contributor V

Hi Eric,

I didn't get anything from Timesys - I just bought  the board from Arrow and it came with that SD card (in a, let's say, poor packaging !!!!).

I've run the image you've pointed and the result is the same:

- U-Boot detects the HD

- Linux says "No sata disk".

root@nitrogen6x:~# uname -a

Linux nitrogen6x 3.0.35-4.1.0+yocto+g5809938 #1 SMP PREEMPT Sat Sep 28 12:11:23 MST 2013 armv7l GNU/Linux

Regards,

Gonzalo.

0 Kudos
Reply