WiFi / Ethernet coexistence in Android

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WiFi / Ethernet coexistence in Android

2,182 次查看
andreygelman
Contributor III

I see that in both ICS and JB WiFi and Ethernet cannot coexist.

I have quite figured out the reason: ConnectivityService.java manages kind of policy, where all the network connections are prioritized, so the one with the lower priority is torn down (Ethernet happens to be prioritized over WiFi).

When the unrequired network is disconnected (e.g. Ethernet cable is pulled out or WiFi is off), the other network is Ok.

But in order to use my device (i.mx6) as an access point, I would like to have them both.

I have tried to merely delete the policy checks from the code, but, at least with JB, it seems to screw the networking altogether.

How can it be done ?

Thanks in advance,

Andrey

标签 (2)
0 项奖励
回复
1 回复

1,484 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 项奖励
回复