command line doesn't process wildcards, why?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

command line doesn't process wildcards, why?

Jump to solution
4,062 Views
EdSutter
Senior Contributor II

I'm running with iMX6 custom hardware, and have been trying to understand why my system isn't

coming up the way it should.  I tracked this down to find that the line...

for i in /etc/init.d/S??* ;do


isn't substituting the 'S??*' with the files in /etc/init.d.  Then I just tried

ls /bin/m* to see if it would list all files that start with 'm' in /bin.  Even that

fails:

# ls /bin/m*

ls: /bin/m* : No such file or directory

I'm guessing there is some misconfiguration in busybox, but I haven't found anything.

-- EDIT on Jan 13 --

I managed to get this to work but have no clue why...

First, note that I am using buildroot to create my rootfs (kernel and uboot are mainline)...

In my buildroot configuration, I had "Target Architecture Variant" set to cortex-A9 (since I'm working with iMX6).

When I backed this setting off to A8, for some bizarre reason that fixed this issue.

What is it about A8/A9 that would cause regular expression wildcard processing in the shell not to work?

I sure would like to understand this one.

-- End EDIT --

Anyone ever have to deal with this ?

Tx

Ed

Message was edited by: Ed Sutter

Labels (2)
0 Kudos
Reply
1 Solution
3,602 Views
EdSutter
Senior Contributor II

Ok, I think I've got this figured out, but its shakey...

I use buildroot to create my rootfs, and it uses the command line option "-m tune cortex-A9" when building.

For both u-boot (denx) and kernel (freescale git) that option is not used, so I tried manually removing it from

the buildroot scripts...

That fixed it. I can now configure buildroot with cortex-A9 target architecture and the above issue is gone.

Not 100% sure why... is there a bug in "-m tune cortex-A9" with the codesourcery tools?

Or is it possibly an option that must be used for kernel as well? 

Has anyone ever used this option?

BTW, I'm using Sourcery CodeBench ARM 2013.05.

View solution in original post

0 Kudos
Reply
5 Replies
3,603 Views
EdSutter
Senior Contributor II

Ok, I think I've got this figured out, but its shakey...

I use buildroot to create my rootfs, and it uses the command line option "-m tune cortex-A9" when building.

For both u-boot (denx) and kernel (freescale git) that option is not used, so I tried manually removing it from

the buildroot scripts...

That fixed it. I can now configure buildroot with cortex-A9 target architecture and the above issue is gone.

Not 100% sure why... is there a bug in "-m tune cortex-A9" with the codesourcery tools?

Or is it possibly an option that must be used for kernel as well? 

Has anyone ever used this option?

BTW, I'm using Sourcery CodeBench ARM 2013.05.

0 Kudos
Reply
3,602 Views
YixingKong
Senior Contributor IV

Ed

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 Kudos
Reply
3,602 Views
EdSutter
Senior Contributor II

Yixing,

I did resolve this, but as has been the case with a few other questions I post to the forum, I answered it myself (see above).

I've done it a few times with other questions that I've self-answered; but I hesitate to mark my own response as the "correct answer".

I guess I'll just do that so you can manage the state of the question better...

Ed

0 Kudos
Reply
3,602 Views
LeonardoSandova
Specialist I

which shell are you running? (echo $0)

Leo

0 Kudos
Reply
3,602 Views
EdSutter
Senior Contributor II

Leo,

(resending this worded differently to see if my recent failures were caused by the forum's spam filter...)

"echo $0" just shows -sh.  According to busybox menuconfig, it appears to be ash.

Ed

0 Kudos
Reply