How to create lib files with codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create lib files with codewarrior

Jump to solution
4,597 Views
jimtom
Contributor I

How to create lib files with codewarrior

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,314 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
6 Replies
4,314 Views
BlackNight
NXP Employee
NXP Employee

Hello,

with MCU10.3 there is library option available in the wizard.

Otherwise: see

Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse

I hope this helps.

0 Kudos
Reply
4,314 Views
jimtom
Contributor I

not found library option available in the wizard

0 Kudos
Reply
4,314 Views
BlackNight
NXP Employee
NXP Employee

Have you selected a Kinetis device?

It is available for me both in MCU10.4 and MCU10.3.

Maybe you are using an older version?

0 Kudos
Reply
4,314 Views
jimtom
Contributor I

I use MCU10.3.

0 Kudos
Reply
4,314 Views
jimtom
Contributor I

not found library option available in the wizard

1.JPG

0 Kudos
Reply
4,314 Views
BlackNight
NXP Employee
NXP Employee

Select 'Bareboard project' and then it is here:

http://mcuoneclipse.files.wordpress.com/2013/02/library-creation.png

0 Kudos
Reply