Dear All
I am running the (unmodified) Freescale Android R13.4.1 Demo-Image on a SabreSD board with i.MX6Q (TO 1.2) connected to a 100 MBit Ethernet and I am experiencing catastrophic and wildly varying ping-latencies (pinging a server in our local ethernet):
root@android:/ # busybox ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:02:33:C7
inet addr:172.20.26.244 Bcast:172.20.255.255 Mask:255.255.0.0
inet6 addr: fe80::204:9fff:fe02:33c7/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:17 errors:0 dropped:0 overruns:0 frame:0
TX packets:9 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:1847 (1.8 KiB) TX bytes:991 (991.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:64 errors:0 dropped:0 overruns:0 frame:0
TX packets:64 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:4608 (4.5 KiB) TX bytes:4608 (4.5 KiB)
root@android:/ # ping 172.20.8.205
PING 172.20.8.205 (172.20.8.205) 56(84) bytes of data.
64 bytes from 172.20.8.205: icmp_seq=1 ttl=64 time=10.5 ms
64 bytes from 172.20.8.205: icmp_seq=2 ttl=64 time=8.65 ms
64 bytes from 172.20.8.205: icmp_seq=3 ttl=64 time=16.6 ms
64 bytes from 172.20.8.205: icmp_seq=4 ttl=64 time=24.6 ms
64 bytes from 172.20.8.205: icmp_seq=5 ttl=64 time=12.6 ms
64 bytes from 172.20.8.205: icmp_seq=6 ttl=64 time=0.599 ms
64 bytes from 172.20.8.205: icmp_seq=7 ttl=64 time=9.97 ms
64 bytes from 172.20.8.205: icmp_seq=8 ttl=64 time=8.70 ms
64 bytes from 172.20.8.205: icmp_seq=9 ttl=64 time=16.6 ms
64 bytes from 172.20.8.205: icmp_seq=10 ttl=64 time=44.6 ms
64 bytes from 172.20.8.205: icmp_seq=11 ttl=64 time=2.72 ms
64 bytes from 172.20.8.205: icmp_seq=12 ttl=64 time=30.6 ms
64 bytes from 172.20.8.205: icmp_seq=13 ttl=64 time=0.283 ms
^C
--- 172.20.8.205 ping statistics ---
13 packets transmitted, 13 received, 0% packet loss, time 12021ms
rtt min/avg/max/mdev = 0.283/14.425/44.657/12.168 ms
root@android:/ # ping 172.20.8.205
PING 172.20.8.205 (172.20.8.205) 56(84) bytes of data.
64 bytes from 172.20.8.205: icmp_seq=1 ttl=64 time=2.67 ms
64 bytes from 172.20.8.205: icmp_seq=2 ttl=64 time=1.79 ms
64 bytes from 172.20.8.205: icmp_seq=3 ttl=64 time=0.327 ms
64 bytes from 172.20.8.205: icmp_seq=4 ttl=64 time=29.9 ms
64 bytes from 172.20.8.205: icmp_seq=5 ttl=64 time=18.6 ms
64 bytes from 172.20.8.205: icmp_seq=6 ttl=64 time=6.83 ms
64 bytes from 172.20.8.205: icmp_seq=7 ttl=64 time=7.03 ms
64 bytes from 172.20.8.205: icmp_seq=8 ttl=64 time=4.30 ms
64 bytes from 172.20.8.205: icmp_seq=9 ttl=64 time=22.7 ms
64 bytes from 172.20.8.205: icmp_seq=10 ttl=64 time=20.6 ms
64 bytes from 172.20.8.205: icmp_seq=11 ttl=64 time=0.290 ms
64 bytes from 172.20.8.205: icmp_seq=12 ttl=64 time=8.85 ms
64 bytes from 172.20.8.205: icmp_seq=13 ttl=64 time=8.35 ms
64 bytes from 172.20.8.205: icmp_seq=14 ttl=64 time=6.70 ms
64 bytes from 172.20.8.205: icmp_seq=15 ttl=64 time=4.66 ms
64 bytes from 172.20.8.205: icmp_seq=16 ttl=64 time=12.6 ms
64 bytes from 172.20.8.205: icmp_seq=17 ttl=64 time=0.834 ms
64 bytes from 172.20.8.205: icmp_seq=18 ttl=64 time=9.69 ms
64 bytes from 172.20.8.205: icmp_seq=19 ttl=64 time=7.69 ms
^C
--- 172.20.8.205 ping statistics ---
19 packets transmitted, 19 received, 0% packet loss, time 18026ms
rtt min/avg/max/mdev = 0.290/9.199/29.970/8.071 ms
root@android:/ # ping 172.20.8.205
PING 172.20.8.205 (172.20.8.205) 56(84) bytes of data.
64 bytes from 172.20.8.205: icmp_seq=1 ttl=64 time=2.66 ms
64 bytes from 172.20.8.205: icmp_seq=2 ttl=64 time=1.74 ms
64 bytes from 172.20.8.205: icmp_seq=3 ttl=64 time=29.7 ms
64 bytes from 172.20.8.205: icmp_seq=4 ttl=64 time=17.6 ms
64 bytes from 172.20.8.205: icmp_seq=5 ttl=64 time=6.59 ms
64 bytes from 172.20.8.205: icmp_seq=6 ttl=64 time=4.65 ms
64 bytes from 172.20.8.205: icmp_seq=7 ttl=64 time=12.6 ms
64 bytes from 172.20.8.205: icmp_seq=8 ttl=64 time=0.680 ms
64 bytes from 172.20.8.205: icmp_seq=9 ttl=64 time=0.245 ms
64 bytes from 172.20.8.205: icmp_seq=10 ttl=64 time=49.9 ms
The same problem can be seen on our own i.MX6Q-based board both running Android and Linux. It doesn't seem to make any difference, whether I connect the boards to a 100 MBit switch, to a 1 GBit switch or via cross-link cable directly to the PC that I ping -- pinging different PCs/servers also doesn't make a difference. These latencies also show up with other protocols and tools other than ping. Using a Linux-kernel with power-management completely disabled also shows this behavior. Even a back-port of the "fec.c"-mainline driver from public Linux v3.8.2 kernel sources still shows this problem. Performance is so bad, that during ssh- or telnet-sessions we keep losing the connection and TFTP and FTP downloads occasionally fail.
Performing a ping-test running Windows-CE7 on our own i.MX6Q-board I get ping-times <1ms, though -- even on the very same board, that shows the ping-latency problems in Linux/Android...
Running the same tests in the same network environment on i.MX53-based boards running Linux/Android (Freescale's QSB/Loco-Board as well as our own design) show expected ping-latencies of <0.5ms, as well.
So the reason might probably be somewhere in i.MX6x-specific code in the kernel... Anybody else noticed similar problems or has any clue, what the cause of the problem might be?
Regards,
Marc