Netx TCP multipart not working in http server

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Netx TCP multipart not working in http server

1,483件の閲覧回数
MAUZ
Contributor I

I am using Azure http server using netx library on IMX1064 processor. The Client is posting large data which is spit into multiple TCP packets using HTTP PUT. I have a custom handler on the server side. 

When the multipart data is received, I get only the first PUT packet on the server but the additional packets with multipart boundary do not  show up in the netx http server.

I can see the packets are coming when I sniff the traffic using wireshark.

0 件の賞賛
返信
0 返答(返信)