We have a new i.MX283 / i.MX287 SODIMM sized SOM, the CFA-10036:
Here are the features that set this module apart:
This module has a very low cost of entry. At the minimum level, all you need to use it is the module itself and a standard microUSB cable.
We also have a debug/prototyping board that adds wired Ethernet and USB A connectors, as well as a generous prototyping area:
For the initial production we have this as a project on Kickstarter:
CFA-10036 Open, Hackable, Linux + ARM Embedded GPIO Module
Please contact [email protected] for production inquiries.
| Crystalfontz America, Incorporated
| 12412 East Saltese Avenue
| Spokane Valley, WA 99216-0357
| voice (509) 892-1200 fax (509) 892-1203 US toll-free (888) 206-9720
Very nice board layout! I like the use of the low inductance decoupling caps! I presume this helped save you stacking the multiple caps the reference schematics call for (33uF total)?
> Very nice board layout! I
Thank you for the kind words.
> low inductance decoupling caps
Here is the part we are using:
Capacitors | details for LLL185R71A104MA01# | Murata
I had researched getting low impedance out of the MLCC caps, and using multiple vias is supposed to help reduce the impedance quite a bit. I think having multiple vias along with the "long side" (0306, instead of 0603) capacitors gets the most performance out of the fewest parts.
Here is one paper for reference: