iWave is upgrading Android KitKat 4.4 BSP for its all variants of i.MX6 Qseven SOMs. The KitKat BSP supports following features and will be available in end of Q2 2015:

Besides the Android support, Linux and WEC7 board support packages are also available for the i.MX6 Qseven SOMs from iWave systems. More details about the i.MX6 Qseven SOM & software features can be found in the i.MX6 Qseven product page.
Device drivers will be supported for specific interface chipsets, which are used in iWave's Qseven Carrier board. More details about iWave i.MX6 Qseven development kit can be found in the following webpage: http://www.iwavesystems.com/product/development-platform/i-mx6-q7-development-kit-54.html