iMX RT1062 LPSPI clock incorrect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX RT1062 LPSPI clock incorrect

722 次查看
maxshaffer
Contributor I

I'm not getting the LPSPI clock rate and Delay Between Frames timing that I expect.

maxshaffer_0-1662578228354.png

With an LPSPI functional clock of 96MHz, I believe I should be able to achieve a 24MHz SPI clock (SCK) with a TCR.PRESCALE value of 1 (divide by 2) and a CCR.SCKDIV value of 0 (divide by 0 + 2). This should be 96MHz / 2 / 2 = 24MHz. From my scope capture I see a SPI clock of 20.833MHz.

maxshaffer_4-1662579038867.png

With a functional clock of 96MHz and the TCR.PRESCALE value of 1 (divide by 2), I believe I should be able to achieve a Delay Between Transfers of 5us with a CCR.DBT value of 238. This should be (238 + 2) / (96MHz / 2) = 5us. From my scope capture I see a delay between transfers of 6us.

maxshaffer_3-1662579018479.png

Note, I manually edited the LPSPI_MasterInit() function in the fsl_lpspi.c driver generated by MCUXpresso to force PRESCALE = 1, SCKDIV = 0, and DBT = 238, because the values computed by this function were also wrong. LPSPI_MasterInit computed PRESCALE = 0 (divide by 1), SCKDIV = 2 (divide by 4) and DBT = 255. In this configuration SCK should still be 24MHz as requested, but I still see 20.833MHz on the scope. The DBT value in this case would result in a delay of 3.2us, which is less than requested. Here are my edits...

maxshaffer_1-1662578724506.png

This is how I configured the 96MHz LPSPI_CLK_ROOT.

maxshaffer_5-1662579373465.png

@RussellPead 

0 项奖励
回复
1 回复

689 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Sorry for the later reply.

I check you post another thread [LPSPI & eDMA master RT1060]  about this topic.

Could we do the communication focus on one thread?

Thanks for the understanding.

Mike

0 项奖励
回复