i.MX RT1050 Flashloader source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1050 Flashloader source code

15,910件の閲覧回数
ryanshuttlewort
Contributor IV

Hello all, I am looking for source code for the flashloader.elf/srec binary packaged with the Flashloader_RT1050_1.x.zip archive.  If you know where I can find it please post a link.

P.S. I have had a look at MCUBOOT (aka KBOOT?) but it does not appear to contain a target for the RT105x.

Thanks.

ラベル(1)
タグ(2)
0 件の賞賛
返信
11 返答(返信)

13,350件の閲覧回数
jackking
Senior Contributor I

I downloaded the latest SDK, 2.5.0 with all middleware components. 

Can someone explain the exact folder where the flashloader source lives? (under mcu-boot?)

I was under the impression that "MCUBoot" was a completely separate utility that was pre-installed on the IMXRT ROM.

FlashLoader is a different application that is loaded into RAM after using MCUBoot receives it, so I'm not sure why the source for flashloader would live under mcu-boot.

Is the Flashloader source meant to be compiled directly?  I didn't see any makefiles either.

SDK_2_5_0_EVKB-IMXRT1050_1_.png

0 件の賞賛
返信

13,341件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jack

yes it is under mcu-boot, please check folder  ../targets/MIMXRT1052

and attached i.MX RT1050 Flashloader v2.7.0 Release Notes.pdf in ../doc folder

Best regards
igor

0 件の賞賛
返信

13,340件の閲覧回数
chunleizhang
Contributor I

Hello all, I am also looking for source code for the rt1050 IAP program.

0 件の賞賛
返信

13,341件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

I apologize for the delay.

In the below web-page, you can find the flash loader:

i.MX RT1050 crossover processor| Arm Cortex-M7|NXP 

You only need to download the flash loader from the Recommended Software & Tools part.

Best Regards,

Diego.

0 件の賞賛
返信

13,341件の閲覧回数
rans
Senior Contributor I

Hello,

I also need the source code.

Is it available ?

Thank you,

ran

0 件の賞賛
返信

13,341件の閲覧回数
melissa_hunter
NXP Employee
NXP Employee

Hi Ran,

The flashloader source for RT1050 is available as optional middleware when you install the SDK from https://mcuxpresso.nxp.com/en/builder.

 

In the SDK builder, choose Add Software Component. The flashloader is listed under mcu-boot.

Regards,

Melissa

0 件の賞賛
返信

13,341件の閲覧回数
mariocenteno
NXP Employee
NXP Employee

Hello,

The flashloader is posted in the i.MX RT1050 webpage under software and tools:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-appl...

thanks,

Mario

0 件の賞賛
返信

13,341件の閲覧回数
ryanshuttlewort
Contributor IV

Hello Diego.  The link you posted appears to be the Flashloader distribution archive, not the source code.  I am specifically looking for the source code for all of the tools in this archive.

Thanks.

0 件の賞賛
返信

13,341件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

Flash loader sources will be available soon from the NXP KBOOT web site. 
MCU Bootloader|NXP 


It is planned to be released in the upcoming i.MX RT1050 MCUX-SDK release.


I apologize, but I do not have more details about the exact release date.

Best Regards,

Diego.

0 件の賞賛
返信

13,341件の閲覧回数
yi-yuanting
Contributor III

Hi Diego,

(1) Is there a schedule about the updating of MCU Bootloader? The year of the latest version is still 2016..........

(2) We are developing our product with RT1050, but there are "no" resources about bootloader in hyper flash(for example: source code of flashloader in hyper flash). It's glad to hear that you said the resources will be released in the upcoming SDK, but when will it be release? Is there any advance information about this new RT1050 SDK?? 

Thanks.

Diego Adrian Cuevas 留言:

Hello

 

Flash loader sources will be available soon from the NXP KBOOT web site. 
MCU Bootloader|NXP 


It is planned to be released in the upcoming i.MX RT1050 MCUX-SDK release.


I apologize, but I do not have more details about the exact release date.

 

Best Regards,

Diego.

 

 

0 件の賞賛
返信

13,341件の閲覧回数
admohamed
Contributor I

Hello Diego,

I am looking for the IMXrt1050  bootloader. I went to the site you recommended: MCU Bootloader|NXP.

There is no a bootloader for Imxrt1050. Any idea where I might be able to find it?

Thanks

Adeed

0 件の賞賛
返信