SEMC Initialization for IMXRT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SEMC Initialization for IMXRT

ソリューションへジャンプ
3,500件の閲覧回数
yamakatb
Contributor III

Hello,

MIMXRT1064 is used in IAR SDRAM using EWARM IDE.

My SDRAM manual:
https://www.winbond.com/resource-files/w9825g6jb_a05_20170306.pdf

Question:
I am trying to initialize SEMC in the startup routine. There is SEMC_Init after __low_level_init, pin_mux initialization, clock initialization.
Immediately after setting a break and looking at the memory window, the initialization has not been performed and the memory cannot be filled.

On the other hand, if you perform the same initial processing as above in the main, it will succeed.

Is there any missing processing?

Thanks for any help, thank you.

T.Y.

0 件の賞賛
返信
1 解決策
3,370件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi T. Y.,

   If you want to initialize the SDRAM, you also can refer to the SDK IAR project, configure it in the .mac files:

 pastedImage_1.png

pastedImage_2.png

  More details, you can check the SDK IAR project, sdram item in the workspace.

pastedImage_3.png

Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,371件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi T. Y.,

   If you want to initialize the SDRAM, you also can refer to the SDK IAR project, configure it in the .mac files:

 pastedImage_1.png

pastedImage_2.png

  More details, you can check the SDK IAR project, sdram item in the workspace.

pastedImage_3.png

Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信